4.1.5.15 SYS_PostTask Function
C
INLINE void SYS_PostTask(SYS_TaskId_t taskId)Description
Posts a task to the task manager, which is later processed by the task handler of the corresponding stack layer.
A task is processed in the SYS_RunTask() function.
Parameters
| Param | Description |
|---|---|
| taskId | ID of the posted task. The application's ID is ::APL_TASK_ID. IDs of the tasks are listed in the SYS_TaskId enum. Each task has its own priority and is called only if there is no any task with higher priority. A handler is called when respective task can be run. Each task has its own task handler. Correspondence between tasks and handlers is listed below: \n |
| HAL | HAL_TaskHandler() \n |
| BSP | BSP_TaskHandler() \n |
| MAC_PHY_HWD | MAC_PHY_HWD_TaskHandler() \n |
| MAC_HWI | MAC_HWI_TaskHandler() \n |
| ZGP | ZGP_TaskHandler() \n |
| NWK | NWK_TaskHandler() \n |
| ZDO | ZDO_TaskHandler() \n |
| APS | APS_TaskHandler() \n |
| APL | APL_TaskHandler() \n |
Returns
None