2 Installation
The MPLAB Code Configurator can be installed in two ways: via the Microchip Plugins Update Center or from the Microchip website. The following chapters describe these procedures and also the MCC update process.
2.1 Installing MPLAB® Code Configurator from the Microchip Plugins Update Center
- In the MPLAB X IDE, go to Tools -> Plugins.
- Go to the Available Plugins tab.
- Select MPLAB Code Configurator and click the Install button. See figure below.
- The Plugin installer opens. Click Next and check the Terms and Agreements. After this step, the Plugin installer begins downloading the MCC plugin.
- When the MCC plugin download is complete, MPLAB X IDE will ask to be restarted. Upon restart, the plugin is installed.
- MCC can now be opened on a new or already existing MPLAB X IDE project. See Section 4.1 “Setting Up MPLAB X IDE and Launching MCC.“
2.2 Installing MPLAB® Code Configurator from the Microchip Website
The MCC plugin can also be downloaded from the Microchip website by typing the address www.microchip.com/mcc in a web browser, selecting the Current
Download tab, and downloading the Current Version .zip file.
See Figure 2-2.
- Open MPLAB X IDE.
- Go to Tools -> Plugins.
- Select the Downloaded tab, and click on the Add Plugins... button.
- Navigate to the folder where the
downloaded
.zipfile was extracted and select the MCC plugin. It may have a.nbmfile extension. - Click on the Install button. MPLAB X IDE will ask to be restarted. Upon restart, the plugin is installed. See figure below.
- MCC can now be opened on a new or already existing MPLAB X IDE project. See Section 4.1 “Setting Up MPLAB X IDE and Launching MCC.”
2.3 Updating MPLAB® Code Configurator
When an MCC version newer than the one installed is available, the MPLAB X IDE will display a notification in the bottom right corner of the IDE window. By clicking on it, the plugin update wizard is launched. In the wizard, click on the Install button, and the software will download and install the new MCC plugin version. See figure below.
2.4 Older MPLAB® Code Configurator Versions
Older MCC versions are available at the same www.microchip.com/mcc address, under the Archive Download tab.