5.3 CI/CD Support
MPLAB® ICD 5 In-Circuit Debugger can be used as a hardware test tool for Continuous Integration / Continuous Delivery (or Deployment) because of its network communication capabilities. In MPLAB X IDE, use the CI/CD Wizard to create files for Jenkins-Docker or Docker-only integration. See the CI/CD Wizard in MPLAB X IDE User’s Guide (DS-50003243) or the section in the MPLAB X IDE User’s Guide (DS-50002027) for details on CI/CD and using the wizard.
If Jenkins Pipeline Files are selected for creation in the wizard, the debugger may be included using one of the wizard screens (see table below.)
| Option | Description |
|---|---|
| Enable Hardware Testing | Enable the debugger as a test tool. |
| Configuration to Build and Run on ICD 5 | Select a project configuration that uses the debugger; either default or one dedicated to hardware use. |
| IP Address of ICD 5 | Enter the IP address of the debugger you wish to use. If you do not know the IP address of the debugger, you can use ipconfig or a similar tool to search the system to which the debugger is connected for the address. |
| Enable MPLAB Code Coverage | Enable the MPLAB Code Coverage feature. An MPLAB Analysis Tool Suite license will be required to use this feature. Note: The Code Coverage API plugin must be available on your Jenkins server if coverage reporting is enabled. |
| Scan Output for Unity Test Results | Enable if the configuration builds Unity test runners and the build job should create a report based on the resulting output. For more info on how to write Unity tests see Unity - Getting Started. |