12.8 INT Pin
The INT pin can be used to generate an asynchronous edge-triggered interrupt. This interrupt is
                                    enabled by setting the External Interrupt Enable (INTE) bit. The External
                                    Interrupt Edge Select (INTEDG) bit determines on which
                                    edge the interrupt will occur. When the INTEDG bit is set, the
                                    rising edge will cause the interrupt. When the INTEDG bit is
                                    clear, the falling edge will cause the interrupt. The External
                                    Interrupt Flag (INTF) bit will be set when a
                                    valid edge appears on the INT pin. If the GIE and INTE bits are
                                    also set, the processor will redirect program execution to the
                                    interrupt vector.