31.2.5.1.2 Bus Collision During a Repeated Start Condition
During a Repeated Start condition, a bus collision occurs if:
- A low level is sampled on SDA when SCL goes from low level to high level (see Figure 31-37).
- SCL goes low before SDA is asserted low, indicating that another
            host is attempting to transmit a data ‘1’ (see Figure 31-38).
When the user releases SDA and the pin is allowed to float high, the BRG is loaded with SSPxADD and counts down to zero. The SCL pin is then deasserted and when sampled high, the SDA pin is sampled.
If SDA is low, a bus collision has occurred (i.e., another host is
         attempting to transmit a data ‘0’, see Figure 31-37). If
         SDA is sampled high, the BRG is reloaded and begins counting. If SDA goes from high-to-low
         before the BRG times out, no bus collision occurs because no two hosts can assert SDA at
         exactly the same time.
If SCL goes from high-to-low before the BRG times out and SDA has
         not already been asserted, a bus collision occurs. In this case, another host is attempting
         to transmit a data ‘1’ during the Repeated Start
         condition (see Figure 31-38).
If, at the end of the BRG time-out, both SCL and SDA are still high, the SDA pin is driven low and the BRG is reloaded and begins counting. At the end of the count, regardless of the status of the SCL pin, the SCL pin is driven low and the Repeated Start condition is complete.