7.1 System Arbitration
The system arbiter resolves memory access between the system level selections (i.e., Main,
Interrupt Service Routine) and peripheral selection (e.g., DMA and Scanner) based on user-assigned
priorities. A block diagram of the system arbiter can be found below. Each of the system level and
peripheral selections has its own priority selection registers. Memory access priority is resolved
using the number written to the corresponding Priority registers, '0' being the
highest priority selection and the maximum value being the lowest priority. All system level and
peripheral level selections default to the lowest priority configuration. If the same value is in
two or more Priority registers, priority is given to the higher-listed selection according to the
following table.
0' that cannot be changed. If an
interrupt is desired when an NVM read/write operation is in progress, then the ISR priority level
must be set to '0'. The NVM module priority is ignored when PRLOCKED bit is
cleared.| Selection | Priority Register Reset Value | |
|---|---|---|
| System Level | ISR | 7 |
| MAIN | 7 | |
| Peripheral | DMA1 | 7 |
| DMA2 | 7 | |
| DMA3 | 7 | |
| DMA4 | 7 | |
| SCANNER | 7 | |