48.6.3.5 Recoverable Faults
Recoverable faults can restart or halt the timer/counter. Two faults, called Fault A and Fault B, can trigger recoverable fault actions on the compare channels CC0 and CC1 of the TCC. The compare channels' outputs can be clamped to inactive state either as long as the fault condition is present, or from the first valid fault condition detection on until the end of the timer/counter cycle.
Fault Inputs
The first two channel input events (TCCx_MC_0 and TCCx_MC_1) can be used as Fault A and Fault B inputs, respectively. Event system channels connected to these fault inputs must be configured as asynchronous. The TCC must work in a PWM operation.
Fault Filtering
There are three filters available for both Fault A and Fault B input. They are configured by the corresponding Recoverable Fault Configuration registers (FCTRLA and FCTRLB). The three filters can either be used independently or in any combination.
- Input Filtering
-
When disabled (FCTRLx.FILTERVAL = 0), the action of a fault on the output port is asynchronous. This helps the fault action to be performed on the output of the compare channel, even when the fault is caused by the loss of the system clock. Therefore, when a fault occurs, the system will immediately and asynchronously disable the compare channel output as long as a fault is present. To avoid TCC control block corruption by a glitch on a fault input line, the fault action on the TCC control block (retrigger, capture, etc..) is synchronized on internal clock domain. A digital filter can be enabled and configured by the Fault Filter Value bits in the Fault Configuration registers (FCTRLA.FILTERVAL (FCTRLA <28:24>) and FCTRLB.FILTERVAL (FCTRLB <28:24>)). If the fault width is less than the FILTERVAL (in TCC clock cycles), will be ignored. A valid fault event action on the TCC FSM, will be then delayed by the clock cycles represented by the FILTERVAL.
- Fault Blanking
- This ignores any fault input for a certain time just after
a selected waveform output edge. This can be used to prevent false fault
triggering due to signal bouncing, as shown in the figure below.
Blanking can be enabled by writing an edge triggering configuration to
the Fault A or Fault B Blanking Mode bits in the Recoverable Fault
Configuration registers (FCTRLA.BLANK (FCTRLA <6:5>) or FCTRLB.BLANK
(FCTRLB <6:5>)). The desired duration of the blanking must be written
to the Fault Blanking Time bits (FCTRLA.BLANKVAL (FCTRLA <23:16>) or
FCTRLB.BLANKVAL (FCTRLB <23:16>)).
The blanking time tb is calculated by
Here, fGCLK_TCCx_PRESC is the frequency of the prescaled peripheral clock frequency fGCLK_TCCx.
The prescaler is enabled by writing '1' to the Fault A or Fault B Blanking Prescaler bit (FCTRLA.BLANKPRESC(FCTRLA <15>) or FCTRLB.BLANKPRESC(FCTRLB <15>)). When disabled, fGCLK_TCCx_PRESC=fGCLK_TCCx. When enabled, fGCLK_TCCx_PRESC=fGCLK_TCCx/64.
The maximum blanking time (FCTRLA.BLANKVAL (FCTRLA <23:16>) or FCTRLB.BLANKVAL (FCTRLB <23:16>))= 255) at fGCLK_TCCx=96MHz is 2.67µs (no prescaler) or 170µs (prescaling). For fGCLK_TCCx=1MHz, the maximum blanking time is either 170µs (no prescaling) or 10.9ms (prescaling enabled).
- Fault Qualification
- This is enabled by writing a '1' to the Fault A or Fault B Qualification bit in the Recoverable Fault A or Fault B Configuration register ((FCTRLA.QUAL(FCTRLA <4>) or FCTRLB.QUAL(FCTRLB <4>)). When the recoverable fault qualification is enabled (FCTRLA.QUAL(FCTRLA <4>) =1 or FCTRLB.QUAL(FCTRLB <4>)=1, the fault input is disabled all the time and the corresponding channel output has an inactive level, as shown in the figures below.
Fault Actions
Different fault actions can be configured individually for Fault A and Fault B. Most fault actions are not mutually exclusive; therefore two or more actions can be enabled at the same time to achieve a result that is a combination of fault actions.
- Keep Action
- This is enabled by writing the Fault A or Fault B Keeper bit in the corresponding Recoverable Fault A or Fault B Configuration register (FCTRLA.KEEP(FCTRLA <3>) or FCTRLB.KEEP(FCTRLB <3>) to '1'. When enabled, the corresponding channel output will be clamped to zero as long as the fault condition is present. The clamp will be released on the start of the first cycle after the fault condition is no longer present, see next Figure.
- Restart Action
-
This is enabled by writing the Fault A or Fault B Restart bit in corresponding Recoverable Fault A or Fault B Configuration register (FCTRLA.RESTART(FCTRLA <7>) =1 or FCTRLB.RESTART(FCTRLB <7>) to '1'. When enabled, the timer/counter will be restarted as soon as the corresponding fault condition is present. The ongoing cycle is stopped and the timer/counter starts a new cycle, see Waveform Generation in RAMP1 Operation with Restart Action. In RAMP1 operation, when the new cycle starts, the compare outputs will be clamped to inactive level as long as the fault condition is present.
Note: For RAMP2 operation, when a new timer/counter cycle starts the cycle index will change automatically, see Waveform Generation in RAMP2 Operation with Restart Action. Fault A and Fault B are qualified only during the cycle A and cycle B respectively: Fault A is disabled during cycle B, and Fault B is disabled during cycle A.
- Capture Action
- Several capture actions can be selected by writing the Fault A
or Fault B Capture Action bits in the Fault A or Fault B Control register
(FCTRLA.CAPTURE(FCTRLA <14:12>) or FCTRLB.CAPTURE(FCTRLB
<14:12>). When one of the capture operations is selected, the counter
value is captured when the fault occurs. The following capture operations
are available:
- CAPT - the equivalent to a standard capture operation, for further details refer to Capture Operations
- CAPTMIN - gets the minimum time stamped value: on each new local minimum captured value, an event or interrupt is issued.
- CAPTMAX - gets the maximum time stamped value: on each new local maximum captured value, an event or interrupt (IT) is issued, see Capture Action “CAPTMAX” in the FCTRLA or FCTRLB register.
- LOCMIN - notifies by event or interrupt when a local minimum captured value is detected.
- LOCMAX - notifies by event or interrupt when a local maximum captured value is detected.
- DERIV0 - notifies by event or interrupt when a local extreme captured value is detected, see Capture Action “DERIV0” in the FCTRLA or FCTRLB register.
CCy Content:
In CAPTMIN and CAPTMAX operations, CCy keeps the respective extreme captured values, see Capture Action “CAPTMAX”. In LOCMIN, LOCMAX or DERIV0 operation, CCy follows the counter value at fault time, see Capture Action “DERIV0”.
Before enabling CAPTMIN or CAPTMAX mode of capture, the user must initialize the corresponding CCy register value to a value different from zero (for CAPTMIN) and TOP (for CAPTMAX). If the initial value of the CCy register is zero for CAPTMIN and TOP for CAPTMAX, no captures will be performed using the corresponding channel.
MCy Behaviour:
In LOCMIN and LOCMAX operation, capture is performed on each capture event. The MCy interrupt flag is set only when the captured value is above or equal for LOCMIN and below or equal for LOCMAX to the previous captured value. So interrupt flag is set when a new relative local Minimum (for CAPTMIN) or Maximum (for CAPTMAX) value has been detected. DERIV0 is equivalent to an OR function of (LOCMIN, LOCMAX).
In CAPT operation, capture is performed on each capture event. The MCy interrupt flag is set on each new capture.
In CAPTMIN and CAPTMAX operation, capture is performed only when on capture event time, the counter value is lower (for CAPTMIN) or higher (for CAPMAX) than the last captured value. The MCy interrupt flag is set only when on capture event time, the counter value is greater than or equal (for CAPTMIN), or less than or equal (for CAPTMAX) to the value captured on the previous event. So interrupt flag is set when a new absolute local Minimum (for CAPTMIN) or Maximum (for CAPTMAX) value has been detected.
Interrupt Generation
In CAPT mode, an interrupt is generated on each filtered Fault A and Fault B and each dedicated CCy channel capture counter value. In other modes, an interrupt is only generated on an extreme captured value.
- Hardware Halt Action
-
This is configured by writing 0x1 to the Fault A or Fault B Halt mode bits in the Recoverable Fault A or Fault B Configuration registers (FCTRLA.HALT(FCTRLA <9:8>) or FCTRLB.HALT(FCTRLB <9:8>). When enabled, the timer/counter is halted and the cycle is extended as long as the corresponding fault is present.
The next figure ('Waveform Generation with Halt and Restart Actions') shows an example where both restart action and hardware halt action are enabled for Fault A. The compare channel 0 output is clamped to inactive level as long as the timer/counter is halted. The timer/counter resumes the counting operation as soon as the fault condition is no longer present. As the restart action is enabled in this example, the timer/counter is restarted after the fault condition is no longer present.
The figure after that ('Waveform Generation with Fault Qualification, Halt, and Restart Actions') shows a similar example, but with additionally enabled fault qualification. Here, counting is resumed after the fault condition is no longer present.
Note that in RAMP2 and RAMP2A operations, when a new timer/counter cycle starts, the cycle index will automatically change.
Figure 48-32. Waveform Generation with Halt and Restart Actions Figure 48-33. Waveform Generation with Fault Qualification, Halt, and Restart Actions
- Software Halt Action
-
This action is configured by writing 0x2 to the Fault A and Fault B Halt mode bits in the Recoverable Fault A or Fault B configuration registers (FCTRLA.HALT(FCTRLA <9:8>) or FCTRLB.HALT(FCTRLB <9:8>). Software halt action is similar to hardware halt action, but in order to restart the timer/counter, the corresponding fault condition must not be present anymore, and the corresponding FAULT A or Fault B bit in the STATUS register must be cleared by software. See the following figure.