48.6.2.5 Counter Operation
Depending on the mode of operation, the counter is cleared, reloaded, incremented, or decremented at each TCC clock input (CLK_TCC_COUNT). A counter clear or reload mark the end of current counter cycle and the start of a new one.
The counting direction is set by the Direction bit in the Control B Set/Clear registers (CTRLBSET and CTRLBCLR). If the bit reads zero, it is counting up and if the bit reads one, it is counting down.
The counter will count up or down for each tick (clock or event) until it reaches TOP or ZERO. When it is counting up and TOP is reached, the counter will be set to zero or TOP at the next tick (overflow) and the Overflow Interrupt Flag in the Interrupt Flag Status and Clear register (INTFLAG.OVF) will be set. When down-counting, the counter is reloaded with the TOP value when ZERO is reached (underflow), and INTFLAG.OVF bit is set. When TC is counting down, the COUNT register must be initialized to TOP value (PER or CC0 value depending on the mode).
INTFLAG.OVF bit can be used to trigger an interrupt, a DMA request or an event. An overflow/underflow occurrence (i.e. a compare match with TOP/ZERO) will stop counting if the One-Shot bit in the Control B register is set (CTRLBSET.ONESHOT). The One-Shot feature is explained in the section “Additional Features”.
It is possible to change the counter value (by writing directly in the COUNT register) even when the counter is running.
When starting the TCC, the COUNT value will always be ZERO or TOP, depending on direction set by CTRLBSET.DIR bit (CTRLBSET <0> or CTRLBCLR.DIR bit (CTRLBCLR <0>), unless a different value has been written to it, or the TCC has been stopped at a value other than ZERO or TOP.
The write access has higher priority than count, clear, or reload. The direction of the counter can also be changed during normal operation. See the previous figure.
Stop Command
A stop command can be issued from software by using TCC Command bits in Control B Set register (CMD bits (CTRLBSET <7:5>)=0x2, STOP).
When a stop is detected while the counter is running, and if CTRLA.FCYCLE bit (CTRLA <16>) = 0 the counter stops immediately maintaining its current value, however, if CTRLA.FCYCLE bit (CTRLA <16>)=1, it waits until end of current cycle to stop on a start value.
If the waveform generation operation (WG) is used, all waveforms are set to a state defined in Non-Recoverable State y Output Enable bit and Non- Recoverable State y Output Value bit in the Driver Control register (DRVCTRL.NREy and DRVCTRL.NRVy), and the Stop bit in the Status register is set (STATUS.STOP bit (STATUS <0>)).
Pause Event Action
A pause command can be issued when the stop event action is configured in the Input Event Action 1 bits in Event Control register (EVCTRL.EVACT0 bits (EVCTRL <2:0>)=0x3, STOP).
When a pause is detected, the counter will maintain its current value and all waveforms keep their current state when (CTRLA.FCYCLE (CTRLA <16>)=0), or wait to the end of the current cycle to stop on a start value and all waveforms keep their initial state when (CTRLA.FCYCLE (CTRLA <16>)= 1), until a start event action is detected: Input Event Action 0 bits in Event Control register (EVCTRL.EVACT0 bits (EVCTRL <2:0>) = 0x3, START).
Re-Trigger Command and Event Action
A re-trigger command can be issued from software by using TCC Command bits in Control B Set register (CTRLBSET.CMD (CTRLBSET <7:5>)=0x1, RETRIGGER), or from event when the re-trigger event action is configured in the Input Event 0/1 Action bits in Event Control register (EVCTRL.EVACT0 bits (EVCTRL <2:0>)=0x1, RETRIGGER and EVCTRL.EVACT1 bits (EVCTRL <5:3>) =0x1, RETRIGGER).
When the command is detected during counting operation, the counter will be reloaded or cleared, depending on the counting direction (CTRLBSET.DIR (CTRLBSET <0>) or (CTRLBCLR.DIR (CTRLBCLR <0>)). The Re-Trigger bit in the Interrupt Flag Status and Clear register will be set (TRG bit (INTFLAG <1>)). It is also possible to generate an event by writing a '1' to the Re-Trigger Event Output Enable bit in the Event Control register (EVCTRL.TRGEO bit (EVCTRL <9>)). If the re-trigger command is detected when the counter is stopped, the counter will resume counting operation from the value in COUNT.
When a re-trigger event action is configured in the Event Action bits in the Event Control register (EVCTRL.EVACT0 bits (EVCTRL <2:0>)=0x1, RETRIGGER), enabling the counter will not start the counter. The counter will start on the next incoming event and restart on corresponding following event.
Start Event Action
The start action can be selected in the Event Control register (EVCTRL.EVACT0 (EVCTRL <2:0>)=0x3, START) and can start the counting operation when previously stopped. The event has no effect if the counter is already counting. When the module is enabled, the counter operation starts when the event is received or when a re-trigger software command is applied.
When a start event action is configured in the Event Action bits in the Event Control register (EVCTRL.EVACT0 (EVCTRL <2:0>)=0x3, START), enabling the counter will not start the counter. The counter will start on the next incoming event, but it will not restart on subsequent events.
Count Event Action
The TCC can count events. When an event is received, the counter increases or decreases the value, depending on direction settings (CTRLBSET.DIR (CTRLBSET <0>) or CTRLBCLR.DIR (CTRLBCLR <0>)).
The count event action is selected by the Event Action 0 bit group in the Event Control register (EVCTRL.EVACT0 (EVCTRL <2:0>)=0x5, COUNT).
Direction Event Action
The direction event action can be selected in the Event Control register (EVCTRL.EVACT1 (EVCTRL <5:3>)=0x2, DIR). When this event is used, the asynchronous event path specified in the event system must be configured or selected. The direction event action can be used to control the direction of the counter operation, depending on external events level. When received, the event level overrides the Direction settings (CTRLBSET.DIR (CTRLBSET <0>) or CTRLBCLR.DIR (CTRLBCLR <0>)) and the direction bit value is updated accordingly.
Increment Event Action
The increment event action can be selected in the Event Control register (EVCTRL.EVACT0 (EVCTRL <2:0>)=0x4, INC) and can change the Counter state when an event is received. When the TCCx_EV_0 (TCE0) event is received, the counter increments, irrespective of direction setting (CTRLBSET.DIR (CTRLBSET <0>) or CTRLBCLR.DIR (CTRLBCLR <0>)).
Decrement Event Action
The decrement event action can be selected in the Event Control register (EVCTRL.EVACT1 (EVCTRL <5:3>)=0x4, DEC) and can change the Counter state when an event is received. When the TCCx_EV_1 (TCE1) event is received, the counter decrements, irrespective of direction setting (CTRLBSET.DIR (CTRLBSET <0>) or CTRLBCLR.DIR (CTRLBCLR <0>)).
Non-recoverable Fault Event Action
Non-recoverable fault actions can be selected in the Event Control register (EVCTRL.EVACTn=0x7, FAULT). When received, the counter will be stopped and the output of the compare channels is overridden according to the Driver Control register settings (DRVCTRL.NREy and DRVCTRL.NRVy). TCCx_EV_0 input event on TCE0 and TCCx_EV_1 input events on TCE1 must be configured as asynchronous events.
Event Action Off
If the event action is disabled (EVCTRL.EVACTn=0x0, OFF), enabling the counter will also start the counter.