4.3 ADC (PB1)
The ADC input pin is a dedicated pin where the analog signal can be provided as an input
to the RNBD451 module. The RNBD451 module does the ADC conversion using a
fixed reference and provides the digital value that can be read using the Read
ADC input voltage (@,4) command. Prior to initiating the Read ADC
input voltage (@,4) command, the user must configure the factors of voltage
detection using the Set ADC Reference Factor
(S@,<hex16>,<hex8>) command. The factors are used to get the
actual ADC voltage. This command expects the reference voltage and bias voltage
percentages as input parameters. For more details, refer to Read ADC Input Voltage (@,4) and Set ADC Reference Factors (S@,<hex16>,<hex8>).
The first step is to supply the analog signal to the PB1 pin, then the Set ADC
Reference Factors (S@,<hex16>,<hex8>) command sets the
reference voltage and bias voltage percentage. Use the Read ADC (@,4)
command to read the voltage.