7.5.4.1 System Requirements
The following are the system requirements:
- Install the Teledyne LeCroy Wireless Protocol Suite (WPS) v2.35 (or later) to the default root path.
- Copy
liveimport.inifrom the Teledyne Lecroy Wireless folder to the btDebugging tool folder. - Connect a UART-to-USB cable (for
example, FTDI cable) to the RXD and TXD pins of the RNBD451 module, then connect to the system.
This COM port needs to be passed as an argument when executing the
Microchip_BLE_Sniffer_Tool.exe.Note: The COM port associated with the UART-to-USB cable.