8.3.1.4.1 Launch the Tool
The following are the steps to launch the Microchip RNBD Utility tool:Figure 8-6. Microchip RNBD Utility Tool Serial DFU Tab Connection Established 
- To launch the tool, double click
RNBD_DFU_OTAPC_Vx.x.x.exe
. - The tool has two separate tabs for each feature. By default, the DFU tab is selected.
- From the COM dropdown option, select the respective COM Port.
- From the “Baud Rate” drop down list, select the baud rate. For example, select 115200.
- Click Connect to continue.
Figure 8-5. Microchip RNBD Utility Tool Serial DFU Tab View - After clicking the Connect button, the following buttons become active:
- Browse
- Update
- Disconnect
- If the connection is successful, the console text log displays the COM port and baud rate.