5.4.3.6 Indicate Service Change (ISC)
Format:
ISC
Command
ISC triggers service indication if there is a
change in the local service in any of the following ways:- Service/Characteristics change
via the
PCandPScommand - Built-in service configuration by
SScommand - Services were removed by
PZcommand
Remote peer devices that are GATT client roles will receive a service changed indication if they have configured the service changed notification Client Characteristic Configuration Descriptor in the GATT service.
| Example: |
| // Issue service changed indication |
| Response: | AOK | // Success |
Err | // No service has been changed |