5.3.4.6 Connect Specific Bonded Device (C<1-8>)

Format: C<1-8>

The RNBD451 module can store the MAC addresses for up to eight bonded devices. The C command provides an easy way to reconnect to any stored device without typing the MAC address of the stored device, if the device uses a public address. When this command is used to reconnect to a bonded device, the RNBD451 module automatically secures the link when the connection is established. To display the list of stored devices, use command LB.

Example:C2// Reconnect to the second stored device
Response:Trying // Start connecting
%CONNECT%// Status string
Err// Syntax error or invalid parameter
%ERR_CONN%// Status string