4.3 ADC (PB1)

The ADC input pin is a dedicated pin where the analog signal can be provided as an input to the RNBD451 module. The RNBD451 module does the ADC conversion using a fixed reference and provides the digital value that can be read using the Read ADC input voltage (@,4) command. Prior to initiating the Read ADC input voltage (@,4) command, the user must configure the factors of voltage detection using the Set ADC Reference Factor (S@,<hex16>,<hex8>) command. The factors are used to get the actual ADC voltage. This command expects the reference voltage and bias voltage percentages as input parameters. For more details, refer to Query Battery Voltage (QBV) and Set Battery Voltage Factors (SBVF,<hex16>,<hex8>).

The first step is to supply the analog signal to the PB1 pin, then the Set ADC Reference Factors (S@,<hex16>,<hex8>) command sets the reference voltage and bias voltage percentage. Use the Read ADC (@,4) command to read the voltage.