5.3 Acknowledge and No-Acknowledge
After each byte of data is received, the receiving device must confirm with the
         transmitting device that it has successfully received the data byte by responding with an
         Acknowledge (ACK). An ACK occurs when the transmitting device releases the SDA line at the
         falling edge of the eighth clock cycle, followed by the receiving device responding with a
         logic ‘0’ throughout the ninth clock cycle’s high period.
When the AT24C16C transmits data to the
         host, the host can indicate that it has finished receiving data and wants to end the
         operation by sending a logic  ‘1’ response to the AT24C16C instead of an ACK response during the ninth clock cycle. This is known as
         a No-Acknowledge (NACK) and is accomplished when the host sends a logic
            ‘1’ during the ninth clock cycle, at which point the AT24C16C will release the SDA line so the host can then generate a
         Stop condition.
The transmitting device, which can be either the bus host or the
         Serial EEPROM, must release the SDA line at the falling edge of the eighth clock cycle to
         allow the receiving device to drive the SDA line to a logic ‘0’ to ACK the
         previous 8-bit word. The receiving device must release the SDA line at the end of the ninth
         clock cycle to allow the transmitter to continue sending new data. A timing diagram is
         provided in Figure 5-1 to better illustrate these
         requirements.