9.5 Init an already configured BR
- Connect the nRF52480 to the Raspberry Pi with a USB cable
- Log in with :
Username : pi
Password : raspberry
- Connect to Wi-Fi (step 7) or Ethernet according to the configuration
- Get the web server’s IP address (“#hostname -I” or “#ifconfig”)
- Open the web server on a PC connected to the network. If the web server doesn’t work, restart the mdns, otbr-agent and otbr-web services (in this order) and reboot the card
- Form a network (step 17) if needed
- Connect the WBZ (step 18)