4.2.1 Architectural Overview
This section describes the AVR core architecture. The main function of the CPU core is to ensure correct program execution. Therefore, the CPU core can access memories, perform calculations, control peripherals and handle interrupts.
To maximize performance and parallelism, the AVR uses a Harvard architecture with separate memories and buses for program and data. Instructions in the program memory are executed with single-level pipelining. While one instruction is being executed, the next instruction is prefetched from the program memory. This concept enables instructions to be executed in every clock cycle. The program memory is in-system reprogrammable Flash memory and ROM.
The fast-access register file contains 32 × 8-bit general purpose working registers with a single clock cycle access time. This allows a single-cycle Arithmetic Logic Unit (ALU) operation. In a typical ALU operation, two operands are output from the register file, the operation is executed and the result is stored in the register file, in one clock cycle.
Six of the 32 registers can be used as three 16-bit indirect address register pointers for data space addressing, enabling efficient address calculations. One of these address pointers can also be used as an address pointer for Look-up Tables in the Flash program memory. Referred to as ‘X,’ ‘Y’ and ‘Z’ registers, these higher 16-bit function registers are described later in this section.
The ALU supports arithmetic and logic operations between registers or between a constant and a register. Single register operations can also be executed in the ALU. After an arithmetic operation, the status register is updated to reflect information about the result of the operation.
The program flow is provided by conditional and unconditional jump and call instructions, which directly address the entire address space. Most AVR instructions have a single 16-bit word format. Every program memory address contains a 16- or 32-bit instruction.
The program memory space is divided in two sections, the boot program section and the application program section. Both sections have dedicated lock bits for write and read/write protection. The Store Program Memory (SPM) instruction that writes into the application Flash memory section must reside in the boot program section.
During interrupts and subroutine calls, the return address of the Program Counter (PC) is stored on the stack. The stack is effectively allocated in the general data SRAM; the stack size is, thus, only limited by the total SRAM size and the usage of the SRAM. All user programs must initialize the Stack Pointer (SP) in the reset routine before subroutines or interrupts are executed. The SP is read/write accessible in the I/O space. The data SRAM can easily be accessed through the five different addressing modes supported in the AVR architecture.
The memory spaces in the AVR architecture are all linear and regular memory maps.
A flexible interrupt module has its control registers in the I/O space with an additional global interrupt enable bit in the status register. All interrupts have a separate interrupt vector in the interrupt vector table. The interrupts have priority in accordance with their interrupt vector position. The lower the interrupt vector address, the higher the priority.
The I/O memory space contains 64 addresses for CPU peripheral functions as control registers, SPI and other I/O functions. The I/O memory can be accessed directly or as the data space locations following those of the register file, 0x20 to 0x5F. In addition, the circuit has extended I/O space from 0x60 to 0x1FF and SRAM, where only the ST/STS/STD and LD/LDS/LDD instructions can be used.