3.5 Hex File Usage
In the hex file, there are two bytes per program word stored in the Intel® INHX32 hex format. Data is stored LSB first and MSB second. Since there are two bytes per word, the addresses in the hex file are two-times the address in the program memory. For example, if the Configuration Word 1 is stored at 8007h, in the hex file this will be referenced as 1000Eh-1000Fh.