In the Customer tab (see the following figure), the ATA8510 configuration tool
reserves some bytes for the M-field and A-field that are transmitted in the first block
of the RF telegram according to the EN13757-4:2005 standard. For more details,
refer to the EN13757-4:2005 Standard.Figure 5-4. Customer Tab – Customer
Settings
As the A-field must be unique for each device, these two values can be set via EEPROM
write.