26.3 PWM Period
The PWM period is specified by the TxPR register. The PWM period can be calculated using the formula of Equation 26-1. It is required to have FOSC/4 as the selected clock input to the timer for correct PWM operation.
PWM Period=[(T2PR)+1]•4•Tosc•(TMR2 Prescale Value)
Note: TOSC = 1/FOSC
When TxTMR is equal to TxPR, the following three events occur on the next increment cycle:
- TxTMR is cleared
- The PWM output is active (Exception: When the PWM duty cycle = 0%, the PWM output will remain inactive)
- The PWMxDCH and PWMxDCL register values are latched into the buffers
Important: The Timer2 postscaler has no effect on the PWM operation.