3.19 PWM Driver

Overview

PWM is used to generate the PWM pulses, this PWM is used to drive motor and other applications.

Features

  • PWM Frequency and the Duty cycle is user configurable, the range of the Frequency value depends on the clock source selected from the Hardware Dependency module (PLIB).
  • Internal timer operates in Synchronization (Sync) or Trigger mode.
  • Sync sources are user configurable, the timer Reset or clear occurs when the input selected by the Sync source is asserted. The Timer immediately begins to count again from zero unless it is held for some other reason.
  • In Trigger operation, the timer is held in Reset until the input selected by Sync source is asserted.

The following waveform represents the PWM output and the effect of Sync source.

Figure . 
The following waveform represents the PWM output and the effect of Trigger source.
Figure . 

3.19.1 Module Documentation

3.19.1.1 PWM Driver

Pulse Width Modulation Driver using dsPIC MCUs.

3.19.1.1.1 Module description

Pulse Width Modulation Driver using dsPIC MCUs.

Data structures
  • struct PWM_INTERFACE

    Structure containing the function pointers of PWM generator driver.

Definitions
Functions
Variables
  • const struct PWM_INTERFACE PWM1

    Structure object of type PWM_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. PWM1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.

3.19.1.1.2 Definition Documentation

PWM1_Deinitialize

#define PWM1_Deinitialize SCCP1_PWM_Deinitialize

This macro defines the Custom Name for SCCP1_PWM_Deinitialize API.

PWM1_Disable

#define PWM1_Disable SCCP1_PWM_Disable

This macro defines the Custom Name for SCCP1_PWM_Disable API.

PWM1_DutyCycleSet

#define PWM1_DutyCycleSet SCCP1_PWM_DutyCycleSet

This macro defines the Custom Name for SCCP1_PWM_DutyCycleSet API.

PWM1_Enable

#define PWM1_Enable SCCP1_PWM_Enable

This macro defines the Custom Name for SCCP1_PWM_Enable API.

PWM1_Initialize

#define PWM1_Initialize SCCP1_PWM_Initialize

This macro defines the Custom Name for SCCP1_PWM_Initialize API.

PWM1_PeriodSet

#define PWM1_PeriodSet SCCP1_PWM_PeriodSet

This macro defines the Custom Name for SCCP1_PWM_PeriodSet API.

PWM1_PWM_CallbackRegister

#define PWM1_PWM_CallbackRegister SCCP1_PWM_CallbackRegister

This macro defines the Custom Name for SCCP1_PWM_CallbackRegister API.

PWM1_SoftwareTriggerSet

#define PWM1_SoftwareTriggerSet SCCP1_PWM_SoftwareTriggerSet

This macro defines the Custom Name for SCCP1_PWM_SoftwareTriggerSet API.

PWM1_Tasks

#define PWM1_Tasks SCCP1_PWM_Tasks

This macro defines the Custom Name for SCCP1_PWM_Tasks API.

3.19.1.1.3 Function Documentation

MCCP9_PWM_DeadTimeSet()

void MCCP9_PWM_DeadTimeSet (size_t deadTimeCount)

Sets the dead time.

Parameters:
in deadTimeCount

- number of cycles of wait time  

Returns:

none

Note:

This API is only available for MCCP instance  

MCCP9_PWM_OutputModeSet()

void MCCP9_PWM_OutputModeSet (enum PWM_OUTPUT_MODES outputMode)

Sets output mode of MCCP.

Parameters:
in outputMode

- mode of operation  

Returns:

none  

Note:

This API is only available for MCCP instance

SCCP1_PWM_Callback()

void SCCP1_PWM_Callback (void )

This is the default callback with weak attribute. The user can override and implement the default callback without weak attribute or can register a custom callback function using SCCP1_PWM_CallbackRegister.

Parameters:
none
Returns:

none

SCCP1_PWM_CallbackRegister()

void SCCP1_PWM_CallbackRegister (void(*)(void) handler)

This function can be used to override default callback and to define custom callback for SCCP1 PWM event.

Parameters:
in handler

- Address of the callback function

Returns:

none  

SCCP1_PWM_Deinitialize()

void SCCP1_PWM_Deinitialize (void )

Deinitializes the SCCP1 to POR values.

Parameters:
none
Returns:

none  

SCCP1_PWM_Disable()

void SCCP1_PWM_Disable (void )

Disables the SCCP1 module.

Parameters:
none
Returns:

none  

SCCP1_PWM_DutyCycleSet()

void SCCP1_PWM_DutyCycleSet (size_t dutyCycleCount)

Sets the ON pulse width.

Parameters:
in dutyCycleCount

- number of cycles of ON time  

Returns:

none  

SCCP1_PWM_Enable()

void SCCP1_PWM_Enable (void )

Enables the SCCP1 module.

Parameters:
none
Returns:

none  

SCCP1_PWM_Initialize()

void SCCP1_PWM_Initialize (void )

Initializes the SCCP1 Pulse driver. This function must be called before any other SCCP1 function is called.

Parameters:
none
Returns:

none  

SCCP1_PWM_PeriodSet()

void SCCP1_PWM_PeriodSet (size_t periodCount)

Sets the cycle width.

Parameters:
in periodCount

- number of clock counts for PWM Period

Returns:

none  

SCCP1_PWM_SoftwareTriggerSet()

void SCCP1_PWM_SoftwareTriggerSet (void )

This function sets the manual trigger.

Parameters:
none
Returns:

none  

SCCP1_PWM_Tasks()

void SCCP1_PWM_Tasks (void )

This function is used to implement the tasks for polled implementations.

Parameters:
none
Returns:

none  

3.19.1.1.4 Enumeration Type Documentation

PWM_OUTPUT_MODES

enum PWM_OUTPUT_MODES

Enumeration containing the output modes of PWM driver.

Note:

Output Modes are available only for MCCP instance

OUTPUT_SCAN_MODE

Output Scan Mode

BRUSH_DC_OUTPUT_FORWARD

Brush DC Output Forward Mode

BRUSH_DC_OUTPUT_REVERSE

Brush DC Output Reverse Mode

HALF_BRIDGE_OUTPUT

Half Bridge Output Mode

PUSH_PULL_OUTPUT

Push Pull Output Mode

STEERABLE_SINGLE_OUTPUT

Steerable Single Output Mode

3.19.1.1.5 Variable Documentation

PWM1

const struct PWM_INTERFACE PWM1

Structure object of type PWM_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. PWM1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.

3.19.2 Data Structure Documentation

3.19.2.1 PWM_INTERFACE Struct Reference

Structure containing the function pointers of PWM generator driver.

3.19.2.1.1 Detailed Description

Structure containing the function pointers of PWM generator driver.

#include <pwm_interface.h>

Data Fields

3.19.2.1.2 Field Documentation

The documentation for this struct was generated from the following file:

source/

pwm_interface.h

CallbackRegister

void(* CallbackRegister) (void(*handler)(void))

Pointer to SCCPx_PWM_CallbackRegister e.g. SCCP1_PWM_CallbackRegister.

DeadTimeSet

void(* DeadTimeSet) (size_t deadTimeCount)

Pointer to SCCPx_PWM_DeadTimeSet e.g. SCCP1_PWM_DeadTimeSet (This feature is hardware dependent)

DutyCycleSet

void(* DutyCycleSet) (size_t dutyCycleCount)

Pointer to SCCPx_PWM_DutyCycleSet e.g. SCCP1_PWM_DutyCycleSet.

Enable

void(* Enable) (void)

Pointer to SCCPx_PWM_Enable e.g. SCCP1_PWM_Enable.

OutputModeSet

void(* OutputModeSet) (enum PWM_OUTPUT_MODES outputMode)

Pointer to SCCPx_PWM_OutputModeSet e.g. SCCP1_PWM_OutputModeSet (This feature is hardware dependent)

PeriodSet

void(* PeriodSet) (size_t periodCount)

Pointer to SCCPx_PWM_PeriodSet e.g. SCCP1_PWM_PeriodSet.

Tasks

void(* Tasks) (void)

Pointer to SCCPx_PWM_Tasks e.g. SCCP1_PWM_Tasks (Supported only in polling mode)

3.19.3 File Documentation

3.19.3.1 source/pwm_interface.h File Reference

#include <stddef.h>
#include "pwm_types.h"

3.19.3.1.1 Data structures

  • struct PWM_INTERFACE

    Structure containing the function pointers of PWM generator driver.

3.19.3.1.2 Detailed Description

PWM Generated Driver Interface Header File

3.19.3.2 source/pwm_types.h File Reference

This is the generated driver types header file for the PWM driver.

3.19.3.2.2 Detailed Description

This is the generated driver types header file for the PWM driver.

PWM Generated Driver Types Header File

3.19.3.3 source/sccp1.h File Reference

This is the generated driver header file for the SCCP1 driver.

#include <stddef.h>
#include "pwm_interface.h"

3.19.3.3.1 Functions

3.19.3.3.2 Macros

3.19.3.3.3 Variables

  • const struct PWM_INTERFACE PWM1

    Structure object of type PWM_INTERFACE with the custom name given by the user in the Melody Driver User interface. The default name e.g. PWM1 can be changed by the user in the MCCP user interface. This allows defining a structure with application specific name using the 'Custom Name' field. Application specific name allows the API Portability.

3.19.3.3.4 Detailed Description

This is the generated driver header file for the SCCP1 driver.

SCCP1 Generated Driver Header File