6 Enabling PDM Microphones using the Device Tree Overlay
Pulse Digital Modulation (PDM) for microphones is a method used to convert an analog signal into a digital signal. The SAMA7G54-EK features four PDM microphones. For more information, refer to the Quad MEMS Microphones section in the SAMA7G54-EK User´s Guide (DS50003273), available on www.microchip.com.
Follow the steps below to use the device tree overlay to enable PDM microphones:
- During booting, stop at
U-Boot level by pressing Enter key to apply the device tree overlay to enable
Quad PDM microphones.
- Edit the bootcmd
environment variable using the edit bootcmd command and apply the
PDMC0 overlay by updating the string bootcmd from
bootcmd=fatload mmc 1:1 0x63000000 sama7g5ek.itb; bootm 0x63000000#kernel_dtbto
bootcmd=fatload mmc 1:1 0x63000000 sama7g5ek.itb; bootm 0x63000000#kernel_dtb#pdmc0.
- To login as the root user, enter root.
This completes enabling PDM microphones with the pdmc0 device tree overlay.