1.4 TCP/IP WEB NET Server SD Card FATFS
The Web Net Server SD Card application creates a HTTP web server on Microchip evaluation board. The FAT FS File System is used for storing the web pages on an external SD Card.
This demonstration uses the HTTPNET server module that supports encrypted communication with NET_PRES layer and third-party TLS service provider (like wolfSSL).
Description
The TCP/IP WEB NET Server SD Card application is based on MPLAB® Harmony 3 TCP/IP Stack.
The Harmony TCP/IP stack is a collection of different network protocols.
The source files of Harmony 3 TCP/IP stack is available here.
The demo is created with MPLAB X IDE and MCC plugin.
MCC Project Graph - TCP/IP WEB NET Server SD Card
The following Project Graph shows the Harmony components included in the TCP/IP WEB NET Server SD Card demo application.

wolfSSL component is added for secure connection which supports TLS.
wolfCrypt module enabled with MD5 and SHA authentication
FILE SYSTEM is added to read and write from the SDMMC( sdcard ) module with FAT file system.
FreeRTOS component is required for RTOS application. For bare-metal (non-RTOS) FreeRTOS component should not be selected.
NOTE - The above diagram contains FreeRTOS component and that is required for RTOS application. For bare-metal(non-RTOS) FreeRTOS component shouldn't be selected.
TCP/IP Configuration - TCP/IP WEB NET Server SD Card
The TCP/IP modules enabled for the demo is shown in the TCP/IP Configuration Overview
More details of TCP/IP Configuration plugin is available here

The Application Layer modules enabled in the demo are as follows:
- Application Layer Modules
- HTTPNET SERVER enables the target board to act as a Web Server.
- DHCP Client to discover the IPv4 address from the nearest DHCP Server.
- DNS Client provides DNS resolution capabilities to the stack.
- ANNOUNCE to discover the Microchip devices within a local network.
- NBNS, NetBIOS Name Service protocol associates host names with IP addresses. This assign of human-name host names to access boards on the same subnet.
- SMTP CLIENT let applications send e-mails to any recipient worldwide.
- SNTP, Simple Network Time Protocol updates its internal time periodically using a pool of public global time servers.
Downloading and Building the application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
This content can also be downloaded using MCC content manager available as part of the MPLAB® X IDE.
Path of the application within the repository is apps\web_net_server_sdcard_fatfs\firmware
To build the application, refer to the following list of demo configurations and open the project using MPLAB X IDE.
| Project Name | Target Device | Development Board | Description |
|---|---|---|---|
| pic32ck_gc01_cult.X | PIC32CK2051GC01144 | PIC32CK GC01 Curiosity Ultra | TCP/IP WEB NET Server SD Card with KSZ8091 Ethernet PHY - Bare Metal |
| pic32ck_gc01_cult_freertos.X | PIC32CK2051GC01144 | PIC32CK GC01 Curiosity Ultra | TCP/IP WEB NET Server SD Card with KSZ8091 Ethernet PHY - FreeRTOS |
Hardware Setup
The target board for running the application is PIC32CK GC01 Curiosity Ultra.
This section provides essential hardware configuration of this target board to run TCP/IP applications.

Board Setup
To set up the hardware, refer to the section Board Setup in PIC32CK GC01 Curiosity Ultra User Guide.
- Connect the micro USB cable from the computer to the DEBUG USB connector on the PIC32CK GC01 Curiosity Ultra Development Board.
- Insert the SD Card into the SD Card slot (which is on backside of the board) as shown above .
- Establish a connection between the router/switch with the PIC32CK GC01 Curiosity Ultra Development Board through the RJ45 connector.
Running the Application
- Open a terminal application on the host computer (like Hyper-terminal or Tera Term).
- Configure the terminal application for serial port connected to USB debug port of the board.
- Set baud rate as 115200 in the terminal application.
- Build and download the application project on the target board.
- Ensure SD card is formatted and loaded with the web pages provided within the /net_apps_pic32ck_sg_gc/apps/web_net_server_sdcard_fatfs/firmware/src/web_pages directory.
- Insert SD Card to the slot on target board.
- Verify the TCP/IP Stack initialization console messages.
Console Start up

If DHCP client is enabled in the demonstration, wait for the DHCP server to assign an IP address for the development board.
This will be printed on the console. Otherwise, the default static IP address will be assigned to the board.
By entering the command netinfo, the response is obtained as shown above.
Web Server Test
- Open a web browser (like Google Chrome, etc).
- Type the board URL in the address bar of web browser (for example, https://mchpboard_eth or https://<ip-address as shown in the console> ).
- The web browser display following web
page

Application features are:
- Dynamic Variables and Real-time Hardware Control - Pressing Switches on target board toggles buttons on web page. Similarly, Clicking on LED symbol in web page can toggle LEDs on target board.
- Form Processing - Input can be handled from the client by the GET and POST methods.
- Authentication - Shows an example of the commonly used restricted access feature.
- Cookies - Shows an example of storing small text strings on the client side.
- Server Side Includes - An example of how SSI can be used to support dynamic content.
- File Uploads - Shows an example of a file upload using the POST method. The HTTP server can accept a user-defined MPFS/MPFS2 image file for web pages.
- Send E-mail - Shows simple SMTP POST methods
- Dynamic DNS - Exercises Dynamic DNS capabilities
- Network Configuration - The MAC address, host name, and IP address of the evaluation kit can be viewed in the Network Configuration page and some configurations can be updated
- MPFS Upload - A new set of web pages can be uploaded to the web server using this feature, which is accessed through https://mchpboard_eth/mpfsupload
Note: For the LED and SWITCH demo functionality, configure the GPIOs connected to LEDs and Switches on target development board, through the Pin Configuration manager in MCC.
Important Notes when using PIC32CK SG01 Curiosity Ultra
If the user is willing to create/port a net application for PIC32CK SG01 Curiosity Ultra board,
then the following configurations/settings are required additionally for running the application and the TCP/IP Stack in Non-Secure region/configuration on a TrustZone device like PIC32CK SG01 Curiosity Ultra:
- All the components/items in the project graph will remain same as in the case of PIC32CK
GC01 Curiosity Ultra, other than RTC peripheral library.
Replace RTC peripheral library with TCC0 peripheral library, as RTC peripheral cannot be configured as Non-Secure, hence we’re choosing another peripheral as it’s replacement which is TCC0 and can be configured as Non-Secure.
- Mark/Select the peripherals used in the project as ‘Non-Secure’ in Arm TrustZone for
Armv8-M Plugin in MCC.
-
Launch Arm TrustZone for Armv8-M by going to the Project Graph tab in MPLAB X IDE and then select Plugins > Arm TrustZone for Armv8-M.
-
Click the Peripheral Configuration tab to configure Peripherals to run in Non-Secure mode.
- For this project, configure/select ETH, SERCOM5, TCC0 and SDMMC0(if used in the project) as Non-Secure Peripherals.
-
- Verify the Interrupt configuration for the peripherals used in the project is
‘Non-Secure’
- Launch NVIC Configuration by selecting Project Graph > Plugins > NVIC Configuration.
- Verify the configuration for the peripherals ETH, SERCOM5, TCC0 and SDMMC0(if used in the project) is ‘Non-Secure’.