4 ASCII Commands
Both the RN4678 and the RN4677 module have an ASCII command interface over the UART that is based on a similar command set. The RN4678 module is a successor to the RN4677 module; therefore, it has more features and improvements with respect to the RN4677 module. The list of the commands introduced in the RN4678 module in comparison with the RN4677 module are available in Table 4-2. Table 4-1 provides the list of RN4677 commands whose function changed in RN4678. Table 4-3 provides the list of the RN4677 commands that are no longer supported by the RN4678 module.
- RN4678 Bluetooth® Dual Mode Module Command Reference User’s Guide (DS50002506)
- RN4677 Bluetooth® 4.0 Dual Mode Module User’s Guide (DS50002377)
|
Command |
RN4677 Function |
RN4678 Function |
|---|---|---|
SQ,<H16> | Sets the data streaming reliability | Sets the features of the RN4678 module |
ST,<H16>,<H16>,<H16>,<H16> | Sets the connection parameters | Sets the connection parameters. The RN4678 module has an additional connection parameter |
SU,<H8> | Sets UART baud rate | Sets the UART baud rate. The parameter setting the baud rate is updated |
GK | Displays current connection status | Displays current connection status. The functionality of values returned are updated |
C<1-8> | Reconnect to previously connected device. The RN4677 module allows four devices | Reconnect to previously connected device. The RN4678 module allows eight devices |
F[,<0-5>[,<hex>]] | Puts the module in Fast Data mode | Inquires Bluetooth® devices in the neighborhood |
IS | Inquiry scan of other Microchip modules | Sets the scan response payload |
X | Display configurations | Terminates a scan operation |
|
Command |
Default |
Function |
|---|---|---|
SDM,<TXT> | RN4678 | Sets the model string in the Bluetooth® Low Energy device information service |
SDN,<TXT> | Microchip | Sets the manufacture string |
SDR,<TXT> | Current RN4678 software version | Sets the software revision of the firmware |
SDS,<TXT> | MAC address of the device | Sets the serial number of the device |
SH,<0,1> | 0 | Enables low-power operation |
SL,<H8> | 02 | Sets the duration of the Bluetooth classic and Bluetooth Low Energy scan operation |
SX,<H8>,<H8> | — | Sets the functions of the individual pins |
SZ,<0-1> | 0 | Controls the beacon-things feature |
&,<Addr> |
— | Assigns random address to local device |
&C |
— | Clears the random address |
&R |
— | Generates a resolvable random address |
IA,<H8>,<Hex>/IB,<H8>,<Hex>/IS, <H8>,<Hex> NA,<H8>,<Hex>/NB,<H8>,<Hex>/NS, <H8>,<Hex> | — | Sets the advertisement, beacon and scan response payload format |
JA,<Address>/JA,<0,1>,<Address> | — | Adds an address to the white list |
JB | — | Adds all bonded devices to the white list |
JC | — | Clears the white list |
JD | — | Displays devices currently in the white list |
U,<Z,1-8> | — | Removes the device from the linked device list |
|
Command |
Function |
Suggested RN4678 Replacement |
|---|---|---|
E | Display extended settings of the device | — |
A | Starts the Bluetooth® Low Energy advertisement | — |
CF,<address> | Connect to <address> and immediately go into Fast Data mode | Command: Set Fast Data mode before using C command |
CFR | Connect to stored remote address and immediately go into Fast Data mode | Command: Set Fast Data mode before using C command |
H | Help command: Displays basic list of commands |
— |
I,<value 1>,<value 2> | Perform an inquiry scan | Command: |
IL[,<H8>,<H16>,<H16>] | Scan for neighborhood Bluetooth Low Energy devices | Command: |
IN<value 1>,<value 2> | Inquiry scan without Bluetooth name | Command: |
IQ | Scans in pairing mode and returns RSSI | Command: |
IS | Inquiry scan of other Microchip modules | Command: |
IR | Inquiry scan based on Class of Device (COD) | Command: |
N,<address> | Removes device from paired device list | — |
O | Displays other settings | — |
S> | Enable/disable command prompt | Command: Enable/disable command prompt |
Apple Support Improvements
As the RN4677, the RN4678 APL modules natively support the service profile required for iOS devices, the iPod Accessory Profile (iAP2) and the COD that allows the discovery and pairing with iOS devices in the Classic Bluetooth mode. To establish a Bluetooth link with an iOS device, the RN4678 needs to be connected to an Apple authentication co-processor via I2C lines.