3 Hardware Connections
The following figure illustrates the reference schematic for connecting the RN4678 module. The RN4677 module (with integral antenna and shield) hardware configuration is fully compatible with the RN4678 hardware configuration.
For the RN4677 module unshielded module (no shield and RF circuitry and antenna), migrating to the RN4678 module needs a redesign in terms of the RF components and antenna. For more details, refer to the RN4678 Bluetooth® Dual Mode Module Command Reference User’s Guide (DS50002506).
Note: In the RN4678, the SW_BTN pin is enabled/disabled by the
SQ command. Refer to the RN4678 Bluetooth® Dual Mode Module
Command Reference User’s Guide (DS50002506) for more details.