4.15 USART - Universal Synchronous and Asynchronous Receiver and Transmitter
4.15.1 Introduction
The Universal Synchronous and Asynchronous serial Receiver and Transmitter (USART) is a fast and flexible serial communication peripheral. The USART supports several different modes of operation that can accommodate multiple types of applications and communication devices.
4.15.2 Supported Device Families
AVR® Dx | AVR® Ex | ATtiny | ATmega |
4.15.3 Required header files:
#include"mcc_generated_files/uart/usart[X].h"
4.15.4 How to use the USART PLIB Driver
For use-cases for the USART, see: 3.5.3 How to use the UART Driver.
The examples there use the portable API interface of the driver, but could easily be modified to directly us the PLIB API.
4.15.5 Module Documentation
4.15.5.1 USART0
This file contains API prototypes and other datatypes for USART0 module.
4.15.5.1.1 Module description
This file contains API prototypes and other datatypes for USART0 module.
Data structures
-
struct usart0_status_t
Functions
-
void USART0_Initialize (void)
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
-
void USART0_Deinitialize (void)
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
-
void USART0_Enable (void)
This API enables the USART0 module.
-
void USART0_Disable (void)
This API disables the USART0 module.
-
void USART0_TxEnable (void)
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
-
void USART0_TxDisable (void)
This API disables the USART0 transmitter.
-
void USART0_RxEnable (void)
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
-
void USART0_RxDisable (void)
This API disables the USART0 Receiver.
-
void USART0_TXInterruptEnable (void)
This API enables the USART0 transmitter interrupt.
-
void USART0_TXInterruptDisable (void)
This API disables the USART0 transmitter interrupt.
-
void USART0_RXInterruptEnable (void)
This API enables the USART0 receiver interrupt.
-
void USART0_RXInterruptDisable (void)
This API disables the USART0 receiver interrupt.
-
bool USART0_IsRxReady (void)
This API checks if USART0 receiver has received data and ready to be read.
-
bool USART0_IsTxReady (void)
This function checks if USART0 transmitter is ready to accept a data byte.
-
bool USART0_IsTxDone (void)
This function return the status of transmit shift register (TSR).
-
uint8_t USART0_ErrotStatusGet (void)
This function gets the error status of the last read byte. This function should be called before USART0_Read().
-
uint8_t USART0_Read (void)
This function reads the 8 bits from receiver FIFO register.
-
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
-
void USART0_FramingErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 framing error.
-
void USART0_OverrunErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 overrun error.
-
void USART0_DefaultErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 default error.
-
void USART0_ParityErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 Parity error.
-
void USART0_TransmitCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Transmitter interrupt.
-
void USART0_ReceiveCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Receiver interrupt.
Variables
4.15.5.1.2 Function Documentation
USART0_DefaultErrorCallbackRegister()
void USART0_DefaultErrorCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon USART0 default error.
|
None. |
USART0_Deinitialize()
void USART0_Deinitialize (void )
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
|
None. |
USART0_Disable()
void USART0_Disable (void )
This API disables the USART0 module.
|
None. |
USART0_Enable()
void USART0_Enable (void )
This API enables the USART0 module.
|
None. |
USART0_ErrotStatusGet()
uint8_t USART0_ErrotStatusGet (void )
This function gets the error status of the last read byte. This function should be called before USART0_Read().
|
Status of the last read byte. See usart0_status_t struct for more details. |
USART0_FramingErrorCallbackRegister()
void USART0_FramingErrorCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon USART0 framing error.
|
None. |
USART0_Initialize()
void USART0_Initialize (void )
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
|
None. |
Section: USART0 APIs
|
None. |
Section: USART0 APIs
USART0_IsRxReady()
bool USART0_IsRxReady (void )
This API checks if USART0 receiver has received data and ready to be read.
|
|
USART0_IsTxDone()
bool USART0_IsTxDone (void )
This function return the status of transmit shift register (TSR).
|
|
USART0_IsTxReady()
bool USART0_IsTxReady (void )
This function checks if USART0 transmitter is ready to accept a data byte.
|
|
USART0_OverrunErrorCallbackRegister()
void USART0_OverrunErrorCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon USART0 overrun error.
|
None. |
USART0_ParityErrorCallbackRegister()
void USART0_ParityErrorCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon USART0 Parity error.
|
None. |
USART0_Read()
uint8_t USART0_Read (void )
This function reads the 8 bits from receiver FIFO register.
The transfer status should be checked to see if the receiver is not empty before calling this function. USART0_IsRxReady() should be checked in if () before calling this API. |
|
8-bit data from RX FIFO register. |
USART0_ReceiveCallbackRegister()
void USART0_ReceiveCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon Receiver interrupt.
|
None. |
USART0_RxDisable()
void USART0_RxDisable (void )
This API disables the USART0 Receiver.
|
None. |
USART0_RxEnable()
void USART0_RxEnable (void )
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
|
None. |
USART0_RXInterruptDisable()
void USART0_RXInterruptDisable (void )
This API disables the USART0 receiver interrupt.
|
None. |
USART0_RXInterruptEnable()
void USART0_RXInterruptEnable (void )
This API enables the USART0 receiver interrupt.
|
None. |
USART0_TransmitCallbackRegister()
void USART0_TransmitCallbackRegister (void(*)(void) callbackHandler)
This API registers the function to be called upon Transmitter interrupt.
|
None. |
USART0_TxDisable()
void USART0_TxDisable (void )
This API disables the USART0 transmitter.
|
None. |
USART0_TxEnable()
void USART0_TxEnable (void )
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
|
None. |
USART0_TXInterruptDisable()
void USART0_TXInterruptDisable (void )
This API disables the USART0 transmitter interrupt.
|
None. |
USART0_TXInterruptEnable()
void USART0_TXInterruptEnable (void )
This API enables the USART0 transmitter interrupt.
|
None. |
USART0_Write()
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
The transfer status should be checked to see if the transmitter is ready to accept a byte before calling this function. USART0_IsTxReady() should be checked in if() before calling this API. |
|
None. |
4.15.5.1.3 Variable Documentation
UART[1/2]
const uart_interface_t UART
External object for usart0_interface.
Section: Data Type Definitions
Section: Driver Interface
Section: Included FilesSection: Macro DeclarationsSection: Driver Interface
UART[1/2]
const uart_interface_t UART
External object for usart0_interface.
Section: Data Type Definitions
Section: Driver Interface
Section: Included FilesSection: Macro DeclarationsSection: Driver Interface
4.15.6 Class Documentation
4.15.6.1 usart0_status_t Struct Reference
4.15.6.1.1 Detailed Description
@breif This is an instance of USART0_STATUS for USART0 module
#include <usart_interrupt.h>
Public Attributes
4.15.6.1.2 Member Data Documentation
The documentation for this struct was generated from the following files:
source/
source/
ferr
unsigned usart0_status_t::ferr
This is a bit field for Framing Error status
oerr
unsigned usart0_status_t::oerr
This is a bit field for Overfrun Error status
perr
unsigned usart0_status_t::perr
This is a bit field for Parity Error status
reserved
unsigned usart0_status_t::reserved
Reserved
status
uint8_t usart0_status_t::status
Group byte for status errors
4.15.7 File Documentation
4.15.7.1 source/usart_interrupt.c File Reference
This is the generated driver implementation file for the USART0 driver using.
#include "../usart0.h"
4.15.7.1.1 Functions
-
static void USART0_DefaultFramingErrorCallback (void)
-
static void USART0_DefaultOverrunErrorCallback (void)
-
static void USART0_DefaultErrorCallback (void)
-
static void USART0_DefaultParityErrorCallback (void)
-
void USART0_TransmitISR (void)
-
void USART0_ReceiveISR (void)
-
void USART0_Initialize (void)
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
-
void USART0_Deinitialize (void)
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
-
void USART0_Enable (void)
This API enables the USART0 module.
-
void USART0_Disable (void)
This API disables the USART0 module.
-
void USART0_TxEnable (void)
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
-
void USART0_TxDisable (void)
This API disables the USART0 transmitter.
-
void USART0_RxEnable (void)
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
-
void USART0_RxDisable (void)
This API disables the USART0 Receiver.
-
void USART0_TXInterruptEnable (void)
This API enables the USART0 transmitter interrupt.
-
void USART0_TXInterruptDisable (void)
This API disables the USART0 transmitter interrupt.
-
void USART0_RXInterruptEnable (void)
This API enables the USART0 receiver interrupt.
-
void USART0_RXInterruptDisable (void)
This API disables the USART0 receiver interrupt.
-
bool USART0_IsRxReady (void)
This API checks if USART0 receiver has received data and ready to be read.
-
bool USART0_IsTxReady (void)
This function checks if USART0 transmitter is ready to accept a data byte.
-
bool USART0_IsTxDone (void)
This function return the status of transmit shift register (TSR).
-
uint8_t USART0_ErrotStatusGet (void)
This function gets the error status of the last read byte. This function should be called before USART0_Read().
-
uint8_t USART0_Read (void)
This function reads the 8 bits from receiver FIFO register.
-
ISR (USART0_RXC_vect)
-
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
-
ISR (USART0_DRE_vect)
-
ISR (USART0_TXC_vect)
-
void USART0_FramingErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 framing error.
-
void USART0_OverrunErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 overrun error.
-
void USART0_DefaultErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 default error.
-
void USART0_ParityErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 Parity error.
-
void USART0_ReceiveCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Receiver interrupt.
-
void USART0_TransmitCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Transmitter interrupt.
4.15.7.1.2 Macros
-
#define USART0_TX_BUFFER_SIZE (8)
-
#define USART0_TX_BUFFER_MASK (USART0_TX_BUFFER_SIZE - 1)
-
#define USART0_RX_BUFFER_SIZE (8)
-
#define USART0_RX_BUFFER_MASK (USART0_RX_BUFFER_SIZE - 1)
4.15.7.1.3 Variables
-
const uart_interface_t UART
External object for usart0_interface.
-
static volatile uint8_t usart0TxHead = 0
-
static volatile uint8_t usart0TxTail = 0
-
static volatile uint8_t usart0TxBuffer [USART0_TX_BUFFER_SIZE]
-
volatile uint8_t usart0TxBufferRemaining
-
static volatile uint8_t usart0RxHead = 0
-
static volatile uint8_t usart0RxTail = 0
-
static volatile uint8_t usart0RxBuffer [USART0_RX_BUFFER_SIZE]
-
static volatile usart0_status_tusart0RxStatusBuffer [USART0_RX_BUFFER_SIZE]
-
volatile uint8_t usart0RxCount
-
static volatile usart0_status_tusart0RxLastError
-
void(* USART0_FramingErrorHandler )(void)
-
void(* USART0_OverrunErrorHandler )(void)
-
void(* USART0_DefaultErrorHandler )(void)
-
void(* USART0_ParityErrorHandler )(void)
-
void(* USART0_TxInterruptHandler )(void)
-
void(* USART0_RxInterruptHandler )(void)
4.15.7.1.4 Detailed Description
This is the generated driver implementation file for the USART0 driver using.
USART0 Generated Driver API Header File
4.15.7.1.5 Macro Definition Documentation
USART0_TX_BUFFER_SIZE
#define USART0_TX_BUFFER_SIZE (8)
Section: Included FilesSection: Macro Declarations
4.15.7.1.6 Variable Documentation
USART0_FramingErrorHandler
void(* USART0_FramingErrorHandler) (void)
Section: USART0 APIs
usart0TxHead
volatile uint8_t usart0TxHead = 0[static]
Section: USART0 variables
4.15.7.2 source/usart_interrupt.h File Reference
#include <stdbool.h> #include <stdint.h> #include <stdio.h> #include "../system/system.h" #include "uart_interface.h"
4.15.7.2.1 Data structures
-
struct usart0_status_t
4.15.7.2.2 Functions
-
void USART0_Initialize (void)
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
-
void USART0_Deinitialize (void)
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
-
void USART0_Enable (void)
This API enables the USART0 module.
-
void USART0_Disable (void)
This API disables the USART0 module.
-
void USART0_TxEnable (void)
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
-
void USART0_TxDisable (void)
This API disables the USART0 transmitter.
-
void USART0_RxEnable (void)
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
-
void USART0_RxDisable (void)
This API disables the USART0 Receiver.
-
void USART0_TXInterruptEnable (void)
This API enables the USART0 transmitter interrupt.
-
void USART0_TXInterruptDisable (void)
This API disables the USART0 transmitter interrupt.
-
void USART0_RXInterruptEnable (void)
This API enables the USART0 receiver interrupt.
-
void USART0_RXInterruptDisable (void)
This API disables the USART0 receiver interrupt.
-
bool USART0_IsRxReady (void)
This API checks if USART0 receiver has received data and ready to be read.
-
bool USART0_IsTxReady (void)
This function checks if USART0 transmitter is ready to accept a data byte.
-
bool USART0_IsTxDone (void)
This function return the status of transmit shift register (TSR).
-
uint8_t USART0_ErrotStatusGet (void)
This function gets the error status of the last read byte. This function should be called before USART0_Read().
-
uint8_t USART0_Read (void)
This function reads the 8 bits from receiver FIFO register.
-
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
-
void USART0_FramingErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 framing error.
-
void USART0_OverrunErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 overrun error.
-
void USART0_DefaultErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 default error.
-
void USART0_ParityErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 Parity error.
-
void USART0_TransmitCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Transmitter interrupt.
-
void USART0_ReceiveCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon Receiver interrupt.
4.15.7.2.3 Macros
-
#define USART0_BAUD_RATE(BAUD_RATE) (((float)4000000 * 64 / (16 * (float)BAUD_RATE)) + 0.5)
-
#define UART_interfaceUART
-
#define UART_InitializeUSART0_Initialize
-
#define UART_DeinitializeUSART0_Deinitialize
-
#define UART_WriteUSART0_Write
-
#define UART_ReadUSART0_Read
-
#define UART__IsRxReadyUSART0_IsRxReady
-
#define UART_IsTxReadyUSART0_IsTxReady
-
#define UART_IsTxDoneUSART0_IsTxDone
-
#define UART_TransmitCallbackRegisterUSART0_TransmitCallbackRegister
-
#define UART_ReceiveCallbackRegisterUSART0_ReceiveCallbackRegister
-
#define UART_FramingErrorCallbackRegisterUSART0_FramingErrorCallbackRegister
-
#define UART_OverrunErrorCallbackRegisterUSART0_OverrunErrorCallbackRegister
-
#define UART_ParityErrorCallbackRegisterUSART0_ParityErrorCallbackRegister
-
#define UART_DefaultErrorCallbackRegisterUSART0_DefaultErrorCallbackRegister
4.15.7.2.4 Variables
-
const uart_interface_t UART
External object for usart0_interface.
4.15.7.2.5 Detailed Description
USART0 Generated Driver API Header File
4.15.7.2.6 Macro Definition Documentation
USART0_BAUD_RATE
#define USART0_BAUD_RATE( BAUD_RATE) (((float)4000000 * 64 / (16 * (float)BAUD_RATE)) + 0.5)
Section: Included Files
4.15.7.3 source/usart_polling.c File Reference
This is the generated driver implementation file for the USART0 driver using.
#include "../usart0.h"
4.15.7.3.1 Functions
-
static void USART0_DefaultFramingErrorCallback (void)
-
static void USART0_DefaultOverrunErrorCallback (void)
-
static void USART0_DefaultErrorCallback (void)
-
static void USART0_DefaultParityErrorCallback (void)
-
void USART0_Initialize (void)
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
-
void USART0_Deinitialize (void)
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
-
void USART0_Enable (void)
This API enables the USART0 module.
-
void USART0_Disable (void)
This API disables the USART0 module.
-
void USART0_TxEnable (void)
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
-
void USART0_TxDisable (void)
This API disables the USART0 transmitter.
-
void USART0_RxEnable (void)
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
-
void USART0_RxDisable (void)
This API disables the USART0 Receiver.
-
bool USART0_IsRxReady (void)
This API checks if USART0 receiver has received data and ready to be read.
-
bool USART0_IsTxReady (void)
This function checks if USART0 transmitter is ready to accept a data byte.
-
bool USART0_IsTxDone (void)
This function return the status of transmit shift register (TSR).
-
uint8_t USART0_ErrotStatusGet (void)
This function gets the error status of the last read byte. This function should be called before USART0_Read().
-
uint8_t USART0_Read (void)
This function reads the 8 bits from receiver FIFO register.
-
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
-
void USART0_FramingErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 framing error.
-
void USART0_OverrunErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 overrun error.
-
void USART0_DefaultErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 default error.
-
void USART0_ParityErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 Parity error.
4.15.7.3.2 Variables
-
const uart_interface_t UART
External object for usart0_interface.
-
static volatile usart0_status_tusart0RxLastError
-
void(* USART0_FramingErrorHandler )(void)
-
void(* USART0_OverrunErrorHandler )(void)
-
void(* USART0_DefaultErrorHandler )(void)
-
void(* USART0_ParityErrorHandler )(void)
4.15.7.3.3 Detailed Description
This is the generated driver implementation file for the USART0 driver using.
USART0 Generated Driver API Header File
4.15.7.3.4 Variable Documentation
USART0_FramingErrorHandler
void(* USART0_FramingErrorHandler) (void)
Section: USART0 APIs
usart0RxLastError
volatile usart0_status_t usart0RxLastError[static]
Section: USART0 variables
4.15.7.4 source/usart_polling.h File Reference
#include <stdbool.h> #include <stdint.h> #include <stdio.h> #include "../system/system.h" #include "uart_interface.h"
4.15.7.4.1 Data structures
-
struct usart0_status_t
4.15.7.4.2 Functions
-
void USART0_Initialize (void)
This API initializes the USART0 driver. This routine initializes the USART0 module. This routine must be called before any other USART0 routine is called. This routine should only be called once during system initialization.
-
void USART0_Deinitialize (void)
This API Deinitializes the USART0 driver. This routine disables the USART0 module.
-
void USART0_Enable (void)
This API enables the USART0 module.
-
void USART0_Disable (void)
This API disables the USART0 module.
-
void USART0_TxEnable (void)
This API enables the USART0 transmitter. USART0 should also be enable to send bytes over TX pin.
-
void USART0_TxDisable (void)
This API disables the USART0 transmitter.
-
void USART0_RxEnable (void)
This API enables the USART0 Receiver. USART0 should also be enable to receive bytes over RX pin.
-
void USART0_RxDisable (void)
This API disables the USART0 Receiver.
-
bool USART0_IsRxReady (void)
This API checks if USART0 receiver has received data and ready to be read.
-
bool USART0_IsTxReady (void)
This function checks if USART0 transmitter is ready to accept a data byte.
-
bool USART0_IsTxDone (void)
This function return the status of transmit shift register (TSR).
-
uint8_t USART0_ErrotStatusGet (void)
This function gets the error status of the last read byte. This function should be called before USART0_Read().
-
uint8_t USART0_Read (void)
This function reads the 8 bits from receiver FIFO register.
-
void USART0_Write (uint8_t txData)
This function writes a byte of data to the transmitter FIFO register.
-
void USART0_FramingErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 framing error.
-
void USART0_OverrunErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 overrun error.
-
void USART0_DefaultErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 default error.
-
void USART0_ParityErrorCallbackRegister (void(*callbackHandler)(void))
This API registers the function to be called upon USART0 Parity error.
4.15.7.4.3 Macros
-
#define USART0_BAUD_RATE(BAUD_RATE) (((float)4000000 * 64 / (16 * (float)BAUD_RATE)) + 0.5)
-
#define UART_interfaceUART
-
#define UART_InitializeUSART0_Initialize
-
#define UART_DeinitializeUSART0_Deinitialize
-
#define UART_WriteUSART0_Write
-
#define UART_ReadUSART0_Read
-
#define UART__IsRxReadyUSART0_IsRxReady
-
#define UART_IsTxReadyUSART0_IsTxReady
-
#define UART_IsTxDoneUSART0_IsTxDone
-
#define UART_TransmitCallbackRegister (NULL)
-
#define UART_ReceiveCallbackRegister (NULL)
-
#define UART_FramingErrorCallbackRegisterUSART0_FramingErrorCallbackRegister
-
#define UART_OverrunErrorCallbackRegisterUSART0_OverrunErrorCallbackRegister
-
#define UART_ParityErrorCallbackRegisterUSART0_ParityErrorCallbackRegister
-
#define UART_DefaultErrorCallbackRegisterUSART0_DefaultErrorCallbackRegister
4.15.7.4.4 Variables
-
const uart_interface_t UART
External object for usart0_interface.
4.15.7.4.5 Detailed Description
USART0 Generated Driver API Header File
4.15.7.4.6 Macro Definition Documentation
USART0_BAUD_RATE
#define USART0_BAUD_RATE( BAUD_RATE) (((float)4000000 * 64 / (16 * (float)BAUD_RATE)) + 0.5)
Section: Included Files