4.3 CCL - Configurable Custom Logic
4.3.1 Introduction
The MCC Melody CCL PLIB Driver (Peripheral Library) generates API to support CCL-specific peripheral functionality on AVRxxxDx and ATtiny target MCU's.
The Configurable Custom Logic (CCL) is a programmable logic peripheral which can be connected to the device pins, events, or other internal peripherals thus serving as the ‘glue logic’ between the device peripherals and external devices. It can eliminate the need for external logic components and can also help the designer to overcome real-time constraints by combining Core Independent Peripherals (CIPs) to handle the most time-critical parts of the application independent of the CPU.
4.3.2 Supported Device Families
AVR® Dx | AVR®EA | ATtiny | ATmega |
4.3.3 Required header files:
#include "mcc_generated_files/ccl/ccl.h"
4.3.4 Module Documentation
4.3.4.1 CCL
This file contains the API prototype for the CCL driver.
4.3.4.1.1 Module description
This file contains the API prototype for the CCL driver.
Functions
int8_t CCL_Initialize (void)
Initializes the CCL. This is called only once during the system initialization.
void LUT0_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT0_OUT interrupt events.
void LUT0_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT0_OUT interrupt event.
void LUT1_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT1_OUT interrupt events.
void LUT1_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT1_OUT interrupt event.
void LUT2_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT2_OUT interrupt events.
void LUT2_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT2_OUT interrupt event.
void LUT3_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT3_OUT interrupt events.
void LUT3_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT3_OUT interrupt event.
void LUT4_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT4_OUT interrupt events.
void LUT4_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT4_OUT interrupt event.
void LUT5_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT5_OUT interrupt events.
void LUT5_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT5_OUT interrupt event.
4.3.4.1.2 Function Documentation
CCL_Initialize()
int8_t CCL_Initialize (void )
Initializes the CCL. This is called only once during the system initialization.
None. |
|
None. |
LUT0_OUT_DefaultInterruptHandler()
void LUT0_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT0_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT0_OUT_SetInterruptHandler()
void LUT0_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT0_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT0_OUT at application runtime
LUT1_OUT_DefaultInterruptHandler()
void LUT1_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT1_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT1_OUT_SetInterruptHandler()
void LUT1_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT1_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT1_OUT at application runtime
LUT2_OUT_DefaultInterruptHandler()
void LUT2_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT2_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT2_OUT_SetInterruptHandler()
void LUT2_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT2_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT2_OUT at application runtime
LUT3_OUT_DefaultInterruptHandler()
void LUT3_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT3_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT3_OUT_SetInterruptHandler()
void LUT3_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT3_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT3_OUT at application runtime
LUT4_OUT_DefaultInterruptHandler()
void LUT4_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT4_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT4_OUT_SetInterruptHandler()
void LUT4_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT4_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT4_OUT at application runtime
LUT5_OUT_DefaultInterruptHandler()
void LUT5_OUT_DefaultInterruptHandler (void )
Default interrupt handler assigned to handle the LUT5_OUT interrupt events.
CCL_Initialize() is already called. |
|
None. |
LUT5_OUT_SetInterruptHandler()
void LUT5_OUT_SetInterruptHandler (void(*)(void) interruptHandler)
Assigns an interrupt handler for the LUT5_OUT interrupt event.
CCL_Initialize() is already called. |
|
None. |
Allows selecting an interrupt handler for LUT5_OUT at application runtime
4.3.5 File Documentation
4.3.5.1 source/ccl.c File Reference
This file contains the API implementations for the CCL driver.
#include "../ccl.h"
4.3.5.1.1 Functions
int8_t CCL_Initialize (void)
Initializes the CCL. This is called only once during the system initialization.
void LUT0_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT0_OUT interrupt event.
void LUT0_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT0_OUT interrupt events.
void LUT1_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT1_OUT interrupt event.
void LUT1_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT1_OUT interrupt events.
void LUT2_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT2_OUT interrupt event.
void LUT2_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT2_OUT interrupt events.
void LUT3_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT3_OUT interrupt event.
void LUT3_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT3_OUT interrupt events.
void LUT4_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT4_OUT interrupt event.
void LUT4_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT4_OUT interrupt events.
void LUT5_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT5_OUT interrupt event.
void LUT5_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT5_OUT interrupt events.
ISR (CCL_CCL_vect)
4.3.5.1.2 Variables
static void(* LUT0_OUT_InterruptHandler )(void)
static void(* LUT1_OUT_InterruptHandler )(void)
static void(* LUT2_OUT_InterruptHandler )(void)
static void(* LUT3_OUT_InterruptHandler )(void)
static void(* LUT4_OUT_InterruptHandler )(void)
static void(* LUT5_OUT_InterruptHandler )(void)
4.3.5.1.3 Detailed Description
This file contains the API implementations for the CCL driver.
CCL Generated Driver File
4.3.5.1.4 Function Documentation
ISR()
ISR (CCL_CCL_vect )
4.3.5.1.5 Variable Documentation
LUT0_OUT_InterruptHandler
void(* LUT0_OUT_InterruptHandler) (void)[static]
LUT1_OUT_InterruptHandler
void(* LUT1_OUT_InterruptHandler) (void)[static]
LUT2_OUT_InterruptHandler
void(* LUT2_OUT_InterruptHandler) (void)[static]
LUT3_OUT_InterruptHandler
void(* LUT3_OUT_InterruptHandler) (void)[static]
LUT4_OUT_InterruptHandler
void(* LUT4_OUT_InterruptHandler) (void)[static]
LUT5_OUT_InterruptHandler
void(* LUT5_OUT_InterruptHandler) (void)[static]
4.3.5.2 source/ccl.h File Reference
#include <stdint.h> #include <stdbool.h> #include "../system/utils/compiler.h"
4.3.5.2.1 Functions
int8_t CCL_Initialize (void)
Initializes the CCL. This is called only once during the system initialization.
void LUT0_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT0_OUT interrupt events.
void LUT0_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT0_OUT interrupt event.
void LUT1_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT1_OUT interrupt events.
void LUT1_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT1_OUT interrupt event.
void LUT2_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT2_OUT interrupt events.
void LUT2_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT2_OUT interrupt event.
void LUT3_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT3_OUT interrupt events.
void LUT3_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT3_OUT interrupt event.
void LUT4_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT4_OUT interrupt events.
void LUT4_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT4_OUT interrupt event.
void LUT5_OUT_DefaultInterruptHandler (void)
Default interrupt handler assigned to handle the LUT5_OUT interrupt events.
void LUT5_OUT_SetInterruptHandler (void(*interruptHandler)(void))
Assigns an interrupt handler for the LUT5_OUT interrupt event.
4.3.5.2.2 Detailed Description
CCL Generated Header File