5.3.2 FUSE bits with three fuse bytes
Fuse Bits with Extended Fuse Byte, Fuse High Byte and Fuse Low Byte
5.3.2.1 Introduction
ATmega32xxx devices have Fuse registers that define the hardware configuration, such as instruction clock speed, watchdog timer, and debug mode. Fuse register bits, also referred to as configuration bits, are changed at programming time with a connected programmer. They are latched in place after the power-up and also at the programming of the device. The Fuse bits has three fuse bytes which can be categorized as extended fuse byte, high fuse byte and low fuse byte.
5.3.2.2 Supported Device Families
ATmega32xx |
5.3.2.3 Required Header Files:
#include "mcc_generated_files/system/config_bits.h"
5.3.2.4 Sample Code
FUSES =
{
.extended = 0x7,
.high = 0xdf ,
.low = 0xa2
}
5.3.2.5 Module Documentation
5.3.2.5.1 CONFIGBITS Driver
This file contains the API Prototypes for the Configuration bits driver.
Module description
This file contains the API Prototypes for the Configuration bits driver.
5.3.2.5.2 System Driver
This file contains the API prototype for the System Driver.
Module description
This file contains the API prototype for the System Driver.
Functions
void SYSTEM_Initialize (void)
Initializes the System module. This routine is called only once during system initialization, before calling any other API.
Function Documentation
SYSTEM_Initialize()
void SYSTEM_Initialize (void )
Initializes the System module. This routine is called only once during system initialization, before calling any other API.
Section: Included Files
None. |
None. |
5.3.2.6 File Documentation
5.3.2.6.1 source/source-files/config_bits.c File Reference
This file contains the API implementation for the Configuration bits driver.
#include <avr/io.h>
Variables
Detailed Description
This file contains the API implementation for the Configuration bits driver.
CONFIGURATION BITS Generated Driver Source File
Variable Documentation
FUSES
FUSES
Initial value:
= { .extended = 0x7, .high = 0xdf , .low = 0xa2 }
Section: Included Files Configures the Fuse bits.
5.3.2.6.2 source/source-files/config_bits.h File Reference
#include "../system/cpu.h"
Detailed Description
CONFIGURATION BITS Generated Driver Header File
5.3.2.6.3 source/source-files/system.c File Reference
This file contains the API implementation for the System driver.
#include "../system.h"
Functions
void SYSTEM_Initialize (void)
Initializes the System module. This routine is called only once during system initialization, before calling any other API.
Detailed Description
This file contains the API implementation for the System driver.
System Driver Source File
5.3.2.6.4 source/source-files/system.h File Reference
#include "../system/utils/compiler.h" #include "config_bits.h" #include "../system/pins.h" #include "../system/cpu.h" #include "../system/cpuint.h"
Functions
void SYSTEM_Initialize (void)
Initializes the System module. This routine is called only once during system initialization, before calling any other API.
Detailed Description
System Driver Header File