4.20.2 16-bit PWM
16-bit Pulse-Width Modulator
4.20.2.1 Introduction
This module is a 16-bit Pulse-Width Modulator (PWM) module that generates a pulse-width modulated signal determined by the duty cycle, period, and resolution.
4.20.2.2 Supported Device Families
| PIC12/16F157x | PIC16F176x | PIC16F177x |
4.20.2.3 Required Header Files
#include "mcc_generated_files/pwm/pwm[x].h"
4.20.2.4 Module Documentation
4.20.2.4.1 PWM1
This is the generated header file for the PWM1 driver.
Module description
This is the generated header file for the PWM1 driver.
Functions
void PWM1_Initialize (void)
Initializes the PWM1 module. This routine is called only once during system initialization, before calling other APIs.
void PWM1_Start (void)
Starts the PWM1 operation and must be called after the initialize routine is called.
void PWM1_Stop (void)
Stops the PWM1 operation and must be called after the start routine is called.
bool PWM1_CheckOutputStatus (void)
Check the output status of the PWM1 module and must be called after the start routine is called.
void PWM1_LoadBufferSet (void)
Loads the PWM1 buffer at the end of the period and must be called after the initialize routine is called.
void PWM1_PhaseSet (uint16_t phaseCount)
Sets the expected phase count for the PWM1 module.
void PWM1_DutyCycleSet (uint16_t dutyCycleCount)
Sets the expected duty cycle for the PWM1 module.
void PWM1_PeriodSet (uint16_t periodCount)
Sets the expected period for the PWM1 module.
void PWM1_OffsetSet (uint16_t offsetCount)
Sets the required offset for the PWM1 module.
uint16_t PWM1_timerCountGet (void)
Reads the measured timer count of the PWM1 module.
bool PWM1_IsOffsetMatchOccured (void)
Gets the status of the Offset Interrupt Flag bit (OFIF) of the PWM1 module.
bool PWM1_IsPhaseMatchOccured (void)
Gets the status of the Phase Interrupt Flag bit (PHIF) of the PWM1 module.
bool PWM1_IsDutyCycleMatchOccured (void)
Gets the status of the Duty Cycle Interrupt Flag bit (DCIF) of the PWM1 module.
bool PWM1_IsPeriodMatchOccured (void)
Gets the status of the Period Interrupt Flag bit (PRIF) of the PWM1 module.
void PWM1_ISR (void)
Implements the Interrupt Servide Routine (ISR) for the PWM1 interrupt. The routine checks which particular interrupt has occurred and calls the respective function.
void PWM1_CallbackRegister (void(*customCallback)(void))
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
Function Documentation
PWM1_CallbackRegister()
void PWM1_CallbackRegister (void(*)(void) customCallback)
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
| (*customCallback)(void) |
- Function pointer to the new callback |
None. |
PWM1_CheckOutputStatus()
bool PWM1_CheckOutputStatus (void )
Check the output status of the PWM1 module and must be called after the start routine is called.
| None. |
True - Output High False - Output Low |
PWM1_DutyCycleSet()
void PWM1_DutyCycleSet (uint16_t dutyCycleCount)
Sets the expected duty cycle for the PWM1 module.
| dutyCycleCount |
- 16-bit duty cycle count |
None. |
PWM1_Initialize()
void PWM1_Initialize (void )
Initializes the PWM1 module. This routine is called only once during system initialization, before calling other APIs.
Section: Included Files Section: PWM1 APIs
| None. |
None. |
PWM1_IsDutyCycleMatchOccured()
bool PWM1_IsDutyCycleMatchOccured (void )
Gets the status of the Duty Cycle Interrupt Flag bit (DCIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMDC value False - PWMTMR count is lower than the PWMDC value |
PWM1_IsOffsetMatchOccured()
bool PWM1_IsOffsetMatchOccured (void )
Gets the status of the Offset Interrupt Flag bit (OFIF) of the PWM1 module.
| None. |
None. |
PWM1_IsPeriodMatchOccured()
bool PWM1_IsPeriodMatchOccured (void )
Gets the status of the Period Interrupt Flag bit (PRIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMPR value False - PWMTMR count is lower than the PWMPR value |
PWM1_IsPhaseMatchOccured()
bool PWM1_IsPhaseMatchOccured (void )
Gets the status of the Phase Interrupt Flag bit (PHIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMPH value False - PWMTMR count is lower than the PWMPH value |
PWM1_ISR()
void PWM1_ISR (void )
Implements the Interrupt Servide Routine (ISR) for the PWM1 interrupt. The routine checks which particular interrupt has occurred and calls the respective function.
| None. |
None. |
PWM1_LoadBufferSet()
void PWM1_LoadBufferSet (void )
Loads the PWM1 buffer at the end of the period and must be called after the initialize routine is called.
| None. |
None. |
PWM1_OffsetSet()
void PWM1_OffsetSet (uint16_t offsetCount)
Sets the required offset for the PWM1 module.
| offsetCount |
- 16-bit offset count |
None. |
PWM1_PeriodSet()
void PWM1_PeriodSet (uint16_t periodCount)
Sets the expected period for the PWM1 module.
| periodCount |
- 16-bit period count |
None. |
PWM1_PhaseSet()
void PWM1_PhaseSet (uint16_t phaseCount)
Sets the expected phase count for the PWM1 module.
| phaseCount |
- 16-bit phase count |
None. |
PWM1_Start()
void PWM1_Start (void )
Starts the PWM1 operation and must be called after the initialize routine is called.
| None. |
None. |
PWM1_Stop()
void PWM1_Stop (void )
Stops the PWM1 operation and must be called after the start routine is called.
| None. |
None. |
PWM1_timerCountGet()
uint16_t PWM1_timerCountGet (void )
Reads the measured timer count of the PWM1 module.
| None. |
16-bit timer count |
4.20.2.5 File Documentation
4.20.2.5.1 source/source-files/pwm1.c File Reference
This is the generated driver implementation file for the PWM1 driver.
#include <xc.h> #include "../pwm1.h"
Functions
static void PWM1_DefaultCallback (void)
Default callback function for interrupt events.
void PWM1_Initialize (void)
Initializes the PWM1 module. This routine is called only once during system initialization, before calling other APIs.
void PWM1_Start (void)
Starts the PWM1 operation and must be called after the initialize routine is called.
void PWM1_Stop (void)
Stops the PWM1 operation and must be called after the start routine is called.
bool PWM1_CheckOutputStatus (void)
Check the output status of the PWM1 module and must be called after the start routine is called.
void PWM1_LoadBufferSet (void)
Loads the PWM1 buffer at the end of the period and must be called after the initialize routine is called.
void PWM1_PhaseSet (uint16_t phaseCount)
Sets the expected phase count for the PWM1 module.
void PWM1_DutyCycleSet (uint16_t dutyCycleCount)
Sets the expected duty cycle for the PWM1 module.
void PWM1_PeriodSet (uint16_t periodCount)
Sets the expected period for the PWM1 module.
void PWM1_OffsetSet (uint16_t offsetCount)
Sets the required offset for the PWM1 module.
uint16_t PWM1_timerCountGet (void)
Reads the measured timer count of the PWM1 module.
bool PWM1_IsOffsetMatchOccured (void)
Gets the status of the Offset Interrupt Flag bit (OFIF) of the PWM1 module.
bool PWM1_IsPhaseMatchOccured (void)
Gets the status of the Phase Interrupt Flag bit (PHIF) of the PWM1 module.
bool PWM1_IsDutyCycleMatchOccured (void)
Gets the status of the Duty Cycle Interrupt Flag bit (DCIF) of the PWM1 module.
bool PWM1_IsPeriodMatchOccured (void)
Gets the status of the Period Interrupt Flag bit (PRIF) of the PWM1 module.
void PWM1_ISR (void)
Implements the Interrupt Servide Routine (ISR) for the PWM1 interrupt. The routine checks which particular interrupt has occurred and calls the respective function.
void PWM1_CallbackRegister (void(*customCallback)(void))
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
Variables
static void(* PWM1_Callback )(void)
Detailed Description
PWM1 Generated Driver API Header File
Function Documentation
PWM1_CallbackRegister()
void PWM1_CallbackRegister (void(*)(void) customCallback)
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
| (*customCallback)(void) |
- Function pointer to the new callback |
None. |
PWM1_DefaultCallback()
static void PWM1_DefaultCallback (void )[static]
Default callback function for interrupt events.
Section: PWM1 APIs
| None. |
None. |
Variable Documentation
PWM1_Callback
void(* PWM1_Callback) (void)[static]
Section: Included Files
4.20.2.5.2 source/source-files/pwm1.h File Reference
#include <stdbool.h> #include <stdint.h>
Functions
void PWM1_Initialize (void)
Initializes the PWM1 module. This routine is called only once during system initialization, before calling other APIs.
void PWM1_Start (void)
Starts the PWM1 operation and must be called after the initialize routine is called.
void PWM1_Stop (void)
Stops the PWM1 operation and must be called after the start routine is called.
bool PWM1_CheckOutputStatus (void)
Check the output status of the PWM1 module and must be called after the start routine is called.
void PWM1_LoadBufferSet (void)
Loads the PWM1 buffer at the end of the period and must be called after the initialize routine is called.
void PWM1_PhaseSet (uint16_t phaseCount)
Sets the expected phase count for the PWM1 module.
void PWM1_DutyCycleSet (uint16_t dutyCycleCount)
Sets the expected duty cycle for the PWM1 module.
void PWM1_PeriodSet (uint16_t periodCount)
Sets the expected period for the PWM1 module.
void PWM1_OffsetSet (uint16_t offsetCount)
Sets the required offset for the PWM1 module.
uint16_t PWM1_timerCountGet (void)
Reads the measured timer count of the PWM1 module.
bool PWM1_IsOffsetMatchOccured (void)
Gets the status of the Offset Interrupt Flag bit (OFIF) of the PWM1 module.
bool PWM1_IsPhaseMatchOccured (void)
Gets the status of the Phase Interrupt Flag bit (PHIF) of the PWM1 module.
bool PWM1_IsDutyCycleMatchOccured (void)
Gets the status of the Duty Cycle Interrupt Flag bit (DCIF) of the PWM1 module.
bool PWM1_IsPeriodMatchOccured (void)
Gets the status of the Period Interrupt Flag bit (PRIF) of the PWM1 module.
void PWM1_ISR (void)
Implements the Interrupt Servide Routine (ISR) for the PWM1 interrupt. The routine checks which particular interrupt has occurred and calls the respective function.
void PWM1_CallbackRegister (void(*customCallback)(void))
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
Detailed Description
PWM1 Generated Driver API Header File
Function Documentation
PWM1_CallbackRegister()
void PWM1_CallbackRegister (void(*)(void) customCallback)
Assigns a callback function that will be called from the ISR when an interrupt event occurs.
| (*customCallback)(void) |
- Function pointer to the new callback |
None. |
PWM1_CheckOutputStatus()
bool PWM1_CheckOutputStatus (void )
Check the output status of the PWM1 module and must be called after the start routine is called.
| None. |
True - Output High False - Output Low |
PWM1_DutyCycleSet()
void PWM1_DutyCycleSet (uint16_t dutyCycleCount)
Sets the expected duty cycle for the PWM1 module.
| dutyCycleCount |
- 16-bit duty cycle count |
None. |
PWM1_Initialize()
void PWM1_Initialize (void )
Initializes the PWM1 module. This routine is called only once during system initialization, before calling other APIs.
Section: Included Files Section: PWM1 APIs
| None. |
None. |
PWM1_IsDutyCycleMatchOccured()
bool PWM1_IsDutyCycleMatchOccured (void )
Gets the status of the Duty Cycle Interrupt Flag bit (DCIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMDC value False - PWMTMR count is lower than the PWMDC value |
PWM1_IsOffsetMatchOccured()
bool PWM1_IsOffsetMatchOccured (void )
Gets the status of the Offset Interrupt Flag bit (OFIF) of the PWM1 module.
| None. |
None. |
PWM1_IsPeriodMatchOccured()
bool PWM1_IsPeriodMatchOccured (void )
Gets the status of the Period Interrupt Flag bit (PRIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMPR value False - PWMTMR count is lower than the PWMPR value |
PWM1_IsPhaseMatchOccured()
bool PWM1_IsPhaseMatchOccured (void )
Gets the status of the Phase Interrupt Flag bit (PHIF) of the PWM1 module.
| None. |
True - PWMTMR count is higher than or equal to the PWMPH value False - PWMTMR count is lower than the PWMPH value |
PWM1_ISR()
void PWM1_ISR (void )
Implements the Interrupt Servide Routine (ISR) for the PWM1 interrupt. The routine checks which particular interrupt has occurred and calls the respective function.
| None. |
None. |
PWM1_LoadBufferSet()
void PWM1_LoadBufferSet (void )
Loads the PWM1 buffer at the end of the period and must be called after the initialize routine is called.
| None. |
None. |
PWM1_OffsetSet()
void PWM1_OffsetSet (uint16_t offsetCount)
Sets the required offset for the PWM1 module.
| offsetCount |
- 16-bit offset count |
None. |
PWM1_PeriodSet()
void PWM1_PeriodSet (uint16_t periodCount)
Sets the expected period for the PWM1 module.
| periodCount |
- 16-bit period count |
None. |
PWM1_PhaseSet()
void PWM1_PhaseSet (uint16_t phaseCount)
Sets the expected phase count for the PWM1 module.
| phaseCount |
- 16-bit phase count |
None. |
PWM1_Start()
void PWM1_Start (void )
Starts the PWM1 operation and must be called after the initialize routine is called.
| None. |
None. |
PWM1_Stop()
void PWM1_Stop (void )
Stops the PWM1 operation and must be called after the start routine is called.
| None. |
None. |
PWM1_timerCountGet()
uint16_t PWM1_timerCountGet (void )
Reads the measured timer count of the PWM1 module.
| None. |
16-bit timer count |