4.15.3 I2C in MSSP
Inter-Integrated Circuit in the Master Synchronous Serial Port
4.15.3.1 Introduction
The Master Synchronous Serial Port (MSSP) peripheral can operate in one of two modes: Serial Peripheral Interface (SPI) and I2C, having the advantage of implementing both communication protocols with the same hardware. The I2C bus is a multi-host serial data communication bus. Devices communicate in a host/client environment where the host devices initiate the communication. A client device is controlled through addressing.
4.15.3.2 Supported Device Families
PIC16F152xx | PIC16(L)F153xx | PIC16(L)F188xx | PIC16F171xx |
PIC16F181xx | PIC16F180xx | PIC16(L)F191xx | PIC16(L)F184xx |
PIC16(L)F183xx | PIC16(L)F193x | PIC16(L)F194x | PIC16(L)F178x |
PIC12(L)F182x | PIC16(L)F182x | PIC12(L)F184x | PIC16(L)F184x |
PIC12(L)F161x | PIC16(L)F161x | PIC12(L)F150x | PIC16(L)F150x |
PIC12LF155x | PIC16LF155x | PIC16LF156x | PIC16LF152x |
PIC16(L)F170x | PIC16(L)F171x | PIC16(L)F176x | PIC16(L)F177x |
PIC16(L)F151x | PIC16(L)F145x | ||
PIC18F-K20 | PIC18F-K22 | PIC18F-K40 | PIC18F-K20 |
PIC18F-K50 | PIC18F-K80 | PIC18F-K90 | PIC18F-Q10 |
4.15.3.3 How to Use the MSSP-I2C PLIB Driver
For use-cases for the I2C mode of the MSSP peripheral, see:
The examples there use the portable API interface of the driver, but could easily be modified to directly us the PLIB API.
4.15.3.4 Module Documentation
4.15.3.4.1 I2C_CLIENT_PLIB
Module description
Modules
-
This file contains other data types for I2C module.
-
This file contains API prototypes and other data types for I2C1 module.
MSSP_CLIENT
This file contains API prototypes and other data types for I2C1 module.
Module description
This file contains API prototypes and other data types for I2C1 module.
Functions
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
void I2C1_WriteByte (uint8_t wrByte)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint8_t I2C1_ReadByte (void)
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint16_t I2C1_ReadAddr (void)
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
i2c_client_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
i2c_client_transfer_dir_t I2C1_TransferDirGet (void)
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
-
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void)
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
-
void I2C1_CallbackRegister (bool(*callback)(i2c_client_transfer_event_t clientEvent))
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
-
void I2C1_ISR (void)
This function is common ISR function for all I2C1 interrupts. I2C1_Initialize() must have been called for the associated.
-
void I2C1_ERROR_ISR (void)
This function is common ISR function for all I2C1 Error interrupts. I2C1_Initialize() must have been called for the associated.
-
void I2C1_Tasks (void)
his function is common Polling function for all I2C1 client. I2C1_Initialize() must have been called for the associated.
Variables
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
Function Documentation
I2C1_CallbackRegister()
void I2C1_CallbackRegister (bool(*)(i2c_client_transfer_event_t clientEvent) callback)
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
|
void |
I2C1_Deinitialize()
void I2C1_Deinitialize (void )
This routine Deinitializes the I2C1 module. This function disables the module.
|
void |
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
|
void |
I2C1_ERROR_ISR()
void I2C1_ERROR_ISR (void )
This function is common ISR function for all I2C1 Error interrupts. I2C1_Initialize() must have been called for the associated.
|
void |
I2C1_ErrorGet()
i2c_client_error_t I2C1_ErrorGet (void )
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
|
I2C_CLIENT_ERROR_BUS_COLLISION - I2C Bus Collision Error I2C_CLIENT_ERROR_WRITE_COLLISION - I2C Write Collision Error I2C_CLIENT_ERROR_RECEIVE_OVERFLOW - I2C Receive overflow I2C_CLIENT_ERROR_NONE - No Error |
This function get the error occurred during I2C Transmit and Receive.
|
I2C_CLIENT_ERROR_BUS_COLLISION - I2C Bus Collision Error I2C_CLIENT_ERROR_WRITE_COLLISION - I2C Write Collision Error I2C_CLIENT_ERROR_RECEIVE_OVERFLOW - I2C Receive overflow I2C_CLIENT_ERROR_NONE - No Error |
|
I2C_ERROR_NONE - No Error I2C_ERROR_NACK - Client returned NACK I2C_ERROR_BUS_COLLISION - Bus Collision Error |
I2C1_Initialize()
void I2C1_Initialize (void )
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
|
void |
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
Section: Public functions
|
void |
Section: Public functions
Section: Public Interfaces
I2C1_ISR()
void I2C1_ISR (void )
This function is common ISR function for all I2C1 interrupts. I2C1_Initialize() must have been called for the associated.
|
void |
I2C1_LastByteAckStatusGet()
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void )
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
|
I2C_CLIENT_ACK_STATUS_RECEIVED_ACK - I2C Host is send ACK to client I2C_CLIENT_ACK_STATUS_RECEIVED_NACK - I2C Host is send NACK to client |
I2C1_ReadAddr()
uint16_t I2C1_ReadAddr (void )
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
|
address byte -I2C1 client read byte |
I2C1_ReadByte()
uint8_t I2C1_ReadByte (void )
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
|
data byte -I2C1 client read byte |
I2C1_Tasks()
void I2C1_Tasks (void )
his function is common Polling function for all I2C1 client. I2C1_Initialize() must have been called for the associated.
|
void. |
I2C1_TransferDirGet()
i2c_client_transfer_dir_t I2C1_TransferDirGet (void )
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
|
I2C_CLIENT_TRANSFER_DIR_WRITE - I2C Host is writing to client I2C_CLIENT_TRANSFER_DIR_READ - I2C Host is reading from client |
I2C1_WriteByte()
void I2C1_WriteByte (uint8_t wrByte)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
|
void |
Variable Documentation
I2C_Client[1/2]
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
Section: Driver Interface
I2C_Client[1/2]
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
Section: Driver Interface
I2C_CLIENT_TYPES
This file contains other data types for I2C module.
Module description
This file contains other data types for I2C module.
Enumerations
-
enum i2c_client_transfer_dir_t { I2C_CLIENT_TRANSFER_DIR_WRITE = 0, I2C_CLIENT_TRANSFER_DIR_READ = 1 }
I2C_CLIENT_TRANSFER_DIR Enumeration.
-
enum i2c_client_ack_status_t { I2C_CLIENT_ACK_STATUS_RECEIVED_ACK = 0, I2C_CLIENT_ACK_STATUS_RECEIVED_NACK = 1 }
I2C Ack/Nack status enumeration.
-
enum i2c_client_transfer_event_t { I2C_CLIENT_TRANSFER_EVENT_NONE = 0, I2C_CLIENT_TRANSFER_EVENT_ADDR_MATCH, I2C_CLIENT_TRANSFER_EVENT_RX_READY, I2C_CLIENT_TRANSFER_EVENT_TX_READY, I2C_CLIENT_TRANSFER_EVENT_STOP_BIT_RECEIVED, I2C_CLIENT_TRANSFER_EVENT_ERROR }
I2C notification event type.
-
enum i2c_client_error_t { I2C_CLIENT_ERROR_NONE = 0, I2C_CLIENT_ERROR_BUS_COLLISION, I2C_CLIENT_ERROR_WRITE_COLLISION, I2C_CLIENT_ERROR_RECEIVE_OVERFLOW, I2C_CLIENT_ERROR_TRANSMIT_UNDERFLOW, I2C_CLIENT_ERROR_READ_UNDERFLOW }
I2C client error type indicator.
Enumeration Type Documentation
i2c_client_ack_status_t
I2C Ack/Nack status enumeration.
I2C_CLIENT_ACK_STATUS_RECEIVED_ACK |
I2C Host is send ACK to client | |
I2C_CLIENT_ACK_STATUS_RECEIVED_NACK |
I2C Host is send NACK to client |
i2c_client_error_t
enum i2c_client_error_t
I2C client error type indicator.
I2C_CLIENT_ERROR_NONE |
I2C error none | |
I2C_CLIENT_ERROR_BUS_COLLISION |
I2C Bus collision occurred | |
I2C_CLIENT_ERROR_WRITE_COLLISION |
I2C Write collision occurred | |
I2C_CLIENT_ERROR_RECEIVE_OVERFLOW |
I2C Receive overflow occurred | |
I2C_CLIENT_ERROR_TRANSMIT_UNDERFLOW |
I2C Trasmit underflow occurred | |
I2C_CLIENT_ERROR_READ_UNDERFLOW |
I2C Receive underflow occurred |
i2c_client_transfer_dir_t
enum i2c_client_transfer_dir_t
I2C_CLIENT_TRANSFER_DIR Enumeration.
I2C_CLIENT_TRANSFER_DIR_WRITE |
I2C Host is writing to client | |
I2C_CLIENT_TRANSFER_DIR_READ |
I2C Host is reading from client |
i2c_client_transfer_event_t
enum i2c_client_transfer_event_t
I2C notification event type.
I2C_CLIENT_TRANSFER_EVENT_NONE |
I2C Bus Idle state | |
I2C_CLIENT_TRANSFER_EVENT_ADDR_MATCH |
Address match event | |
I2C_CLIENT_TRANSFER_EVENT_RX_READY |
Data sent by I2C Host is available | |
I2C_CLIENT_TRANSFER_EVENT_TX_READY |
I2C client can respond to data read request from I2C Host | |
I2C_CLIENT_TRANSFER_EVENT_STOP_BIT_RECEIVED |
I2C stop bit received | |
I2C_CLIENT_TRANSFER_EVENT_ERROR |
I2C Bus error occurred |
4.15.3.4.2 I2C_HOST_PLIB
Module description
Modules
-
This file contains other data types for I2C module.
-
This file contains API prototypes and other data types for I2C1 module.
MSSP_HOST
This file contains API prototypes and other data types for I2C1 module.
Module description
This file contains API prototypes and other data types for I2C1 module.
Functions
-
void I2C1_Initialize (void)
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
-
bool I2C1_Write (uint16_t address, uint8_t *data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_Read (uint16_t address, uint8_t *data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_WriteRead (uint16_t address, uint8_t *writeData, size_t writeLength, uint8_t *readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
-
i2c_host_error_t I2C1_ErrorGet (void)
This function get the error occurred during I2C Transmit and Receive.
-
bool I2C1_IsBusy (void)
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
-
void I2C1_CallbackRegister (void(*callbackHandler)(void))
Setter function for I2C interrupt callback, This will be called when any error is generated.
-
void I2C1_ISR (void)
This function is ISR function for I2C1 Common interrupts.
-
void I2C1_ERROR_ISR (void)
This function is ISR function for I2C1 Error interrupts.
-
void I2C1_Tasks (void)
This is polling function for non interrupt mode.
Variables
Function Documentation
I2C1_CallbackRegister()
void I2C1_CallbackRegister (void(*)(void) callbackHandler)
Setter function for I2C interrupt callback, This will be called when any error is generated.
|
void |
void customI2CCallback(void) { // Custom ISR code } void main(void) { SYSTEM_Initialize(); I2C1_Initialize(); I2C1_CallbackRegister(customI2CCallback); while (!I2C1_WriteRead(0x50, writeData, 1, readData , 2)); while (1) { } }
I2C1_Deinitialize()
void I2C1_Deinitialize (void )
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
|
void |
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
|
void |
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
|
void |
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
|
void |
I2C1_ERROR_ISR()
void I2C1_ERROR_ISR (void )
This function is ISR function for I2C1 Error interrupts.
|
void |
This function is ISR function for I2C1 Error interrupts.
|
void |
I2C1_ErrorGet()
i2c_host_error_t I2C1_ErrorGet (void )
This function get the error occurred during I2C Transmit and Receive.
|
I2C_ERROR_NONE - No Error I2C_ERROR_NACK - Client returned NACK I2C_ERROR_BUS_COLLISION - Bus Collision Error |
This function get the error occurred during I2C Transmit and Receive.
|
I2C_CLIENT_ERROR_BUS_COLLISION - I2C Bus Collision Error I2C_CLIENT_ERROR_WRITE_COLLISION - I2C Write Collision Error I2C_CLIENT_ERROR_RECEIVE_OVERFLOW - I2C Receive overflow I2C_CLIENT_ERROR_NONE - No Error |
|
I2C_ERROR_NONE - No Error I2C_ERROR_NACK - Client returned NACK I2C_ERROR_BUS_COLLISION - Bus Collision Error |
This function get the error occurred during I2C Transmit and Receive.
|
I2C_CLIENT_ERROR_BUS_COLLISION - I2C Bus Collision Error I2C_CLIENT_ERROR_WRITE_COLLISION - I2C Write Collision Error I2C_CLIENT_ERROR_RECEIVE_OVERFLOW - I2C Receive overflow I2C_CLIENT_ERROR_NONE - No Error |
This function get the error occurred during I2C Transmit and Receive.
|
I2C_CLIENT_ERROR_BUS_COLLISION - I2C Bus Collision Error I2C_CLIENT_ERROR_WRITE_COLLISION - I2C Write Collision Error I2C_CLIENT_ERROR_RECEIVE_OVERFLOW - I2C Receive overflow I2C_CLIENT_ERROR_NONE - No Error |
|
I2C_ERROR_NONE - No Error I2C_ERROR_NACK - Client returned NACK I2C_ERROR_BUS_COLLISION - Bus Collision Error |
I2C1_Initialize()
void I2C1_Initialize (void )
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
|
void |
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
Section: Public functions
|
void |
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
Section: Public functions
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
Section: Public Interfaces
I2C1_IsBusy()
bool I2C1_IsBusy (void )
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
|
true - if I2C is busy; false - if I2C is free |
I2C1_ISR()
void I2C1_ISR (void )
This function is ISR function for I2C1 Common interrupts.
|
void |
This function is ISR function for I2C1 Common interrupts.
|
void |
I2C1_Read()
bool I2C1_Read (uint16_t address, uint8_t * data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
The function is non-blocking. It initiates bus activity and returns immediately. The transfer is then completed in the peripheral interrupt. For polling mode, user has to call I2C1_Tasks in while loop. A transfer request cannot be placed when another transfer is in progress. Calling this function when another function is already in progress will cause the function to return false.
|
true - The request was placed successfully and the bus activity was initiated. false - The request fails,if there was already a transfer in progress when this function was called |
I2C1_Tasks()
void I2C1_Tasks (void )
This is polling function for non interrupt mode.
|
void |
This is polling function for non interrupt mode.
|
void. |
I2C1_Write()
bool I2C1_Write (uint16_t address, uint8_t * data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
The function is non-blocking. It initiates bus activity and returns immediately. The transfer is then completed in the peripheral interrupt. For polling mode, user has to call I2C1_Tasks in while loop. A transfer request cannot be placed when another transfer is in progress. Calling this function when another function is already in progress will cause the function to return false.
|
true - The request was placed successfully and the bus activity was initiated. false - The request fails,if there was already a transfer in progress when this function was called |
I2C1_WriteRead()
bool I2C1_WriteRead (uint16_t address, uint8_t * writeData, size_t writeLength, uint8_t * readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
If the Client NAKs the request or a bus error was encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
The function is non-blocking. It initiates bus activity and returns immediately. The transfer is then completed in the peripheral interrupt. For polling mode, user has to call I2C1_Tasks in while loop. A transfer request cannot be placed when another transfer is in progress. Calling this function when another function is already in progress will cause the function to return false.
|
true - The request was placed successfully and the bus activity was initiated. false - The request fails,if there was already a transfer in progress when this function was called |
I2C_HOST_TYPES
This file contains other data types for I2C module.
Module description
This file contains other data types for I2C module.
Data structures
-
struct i2c_host_transfer_setup_t
Structure for i2c clock change.
Enumerations
-
enum i2c_host_error_t { I2C_ERROR_NONE, I2C_ERROR_ADDR_NACK, I2C_ERROR_DATA_NACK, I2C_ERROR_BUS_COLLISION }
Enumeration for I2C errors.
Enumeration Type Documentation
i2c_host_error_t
enum i2c_host_error_t
Enumeration for I2C errors.
I2C_ERROR_NONE |
No Error | |
I2C_ERROR_ADDR_NACK |
Client returned Address NACK | |
I2C_ERROR_DATA_NACK |
Client returned Data NACK | |
I2C_ERROR_BUS_COLLISION |
Bus Collision Error |
4.15.3.5 Class Documentation
4.15.3.5.1 i2c_host_transfer_setup_t Struct Reference
Structure for i2c clock change.
Detailed Description
Structure for i2c clock change.
#include <i2c_host_types.h>
Public Attributes
-
uint32_t clkSpeed
Member Data Documentation
clkSpeed
uint32_t i2c_host_transfer_setup_t::clkSpeed
I2C Clock Speed
4.15.3.6 File Documentation
4.15.3.6.1 source/i2c_client_types.h File Reference
Enumerations
-
enum i2c_client_transfer_dir_t { I2C_CLIENT_TRANSFER_DIR_WRITE = 0, I2C_CLIENT_TRANSFER_DIR_READ = 1 }
I2C_CLIENT_TRANSFER_DIR Enumeration.
-
enum i2c_client_ack_status_t { I2C_CLIENT_ACK_STATUS_RECEIVED_ACK = 0, I2C_CLIENT_ACK_STATUS_RECEIVED_NACK = 1 }
I2C Ack/Nack status enumeration.
-
enum i2c_client_transfer_event_t { I2C_CLIENT_TRANSFER_EVENT_NONE = 0, I2C_CLIENT_TRANSFER_EVENT_ADDR_MATCH, I2C_CLIENT_TRANSFER_EVENT_RX_READY, I2C_CLIENT_TRANSFER_EVENT_TX_READY, I2C_CLIENT_TRANSFER_EVENT_STOP_BIT_RECEIVED, I2C_CLIENT_TRANSFER_EVENT_ERROR }
I2C notification event type.
-
enum i2c_client_error_t { I2C_CLIENT_ERROR_NONE = 0, I2C_CLIENT_ERROR_BUS_COLLISION, I2C_CLIENT_ERROR_WRITE_COLLISION, I2C_CLIENT_ERROR_RECEIVE_OVERFLOW, I2C_CLIENT_ERROR_TRANSMIT_UNDERFLOW, I2C_CLIENT_ERROR_READ_UNDERFLOW }
I2C client error type indicator.
Detailed Description
I2C Generated Driver Types Header File
4.15.3.6.2 source/i2c_host_types.h File Reference
Data structures
-
struct i2c_host_transfer_setup_t
Structure for i2c clock change.
Enumerations
-
enum i2c_host_error_t { I2C_ERROR_NONE, I2C_ERROR_ADDR_NACK, I2C_ERROR_DATA_NACK, I2C_ERROR_BUS_COLLISION }
Enumeration for I2C errors.
Detailed Description
I2C Generated Driver Types Header File
4.15.3.6.3 source/mssp_client_interrupt.c File Reference
This file contains the driver code for I2C1 module.
#include <xc.h> #include "../mssp1.h"
Functions
-
static void I2C1_EventHandler ()
-
static void I2C1_ErrorEventHandler ()
-
static bool I2C1_DefaultCallback (i2c_client_transfer_event_t event)
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
void I2C1_WriteByte (uint8_t data)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint8_t I2C1_ReadByte (void)
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint16_t I2C1_ReadAddr (void)
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
i2c_client_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
i2c_client_transfer_dir_t I2C1_TransferDirGet (void)
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
-
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void)
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
-
void I2C1_CallbackRegister (bool(*callback)(i2c_client_transfer_event_t clientEvent))
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
-
void I2C1_ISR (void)
This function is common ISR function for all I2C1 interrupts. I2C1_Initialize() must have been called for the associated.
-
void I2C1_ERROR_ISR (void)
This function is common ISR function for all I2C1 Error interrupts. I2C1_Initialize() must have been called for the associated.
Variables
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
-
static volatile uint16_t i2c1Addr
-
static volatile i2c_client_error_ti2c1ErrorState
-
static bool(* I2C1_InterruptHandler )(i2c_client_transfer_event_t clientEvent) = NULL
Detailed Description
This file contains the driver code for I2C1 module.
MSSP1 Generated Driver File
Function Documentation
I2C1_EventHandler()
static void I2C1_EventHandler (void )[static]
Section: Private functions declaration
Section: Private functions
Variable Documentation
i2c1Addr
volatile uint16_t i2c1Addr[static]
Section: Private Variable Definitions
4.15.3.6.4 source/mssp_client_interrupt.h File Reference
#include <stdbool.h> #include <stdint.h> #include "i2c_client_interface.h"
Functions
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
void I2C1_WriteByte (uint8_t wrByte)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint8_t I2C1_ReadByte (void)
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint16_t I2C1_ReadAddr (void)
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
i2c_client_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
i2c_client_transfer_dir_t I2C1_TransferDirGet (void)
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
-
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void)
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
-
void I2C1_CallbackRegister (bool(*callback)(i2c_client_transfer_event_t clientEvent))
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
-
void I2C1_ISR (void)
This function is common ISR function for all I2C1 interrupts. I2C1_Initialize() must have been called for the associated.
-
void I2C1_ERROR_ISR (void)
This function is common ISR function for all I2C1 Error interrupts. I2C1_Initialize() must have been called for the associated.
Macros
-
#define I2C_Client_InitializeI2C1_Initialize
-
#define I2C_Client_DeinitializeI2C1_Deinitialize
-
#define I2C_Client_WriteByteI2C1_WriteByte
-
#define I2C_Client_ReadByteI2C1_ReadByte
-
#define I2C_Client_ReadAddrI2C1_ReadAddr
-
#define I2C_Client_ErrorGetI2C1_ErrorGet
-
#define I2C_Client_TransferDirGetI2C1_TransferDirGet
-
#define I2C_Client_LastByteAckStatusGetI2C1_LastByteAckStatusGet
-
#define I2C_Client_CallbackRegisterI2C1_CallbackRegister
-
#define I2C_Client_TasksI2C1_Tasks
Variables
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
Detailed Description
MSSP1 Generated Driver API Header File
Macro Definition Documentation
i2c_client_client_interface
#define i2c_client_client_interface I2C_Client
Section: Data Type Definitions
4.15.3.6.5 source/mssp_client_polling.c File Reference
This file contains the driver code for I2C1 module.
#include <xc.h> #include "../mssp1.h"
Functions
-
static void I2C1_EventHandler ()
-
static void I2C1_ErrorEventHandler ()
-
static bool I2C1_DefaultCallback (i2c_client_transfer_event_t event)
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
void I2C1_WriteByte (uint8_t data)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint8_t I2C1_ReadByte (void)
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint16_t I2C1_ReadAddr (void)
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
i2c_client_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
i2c_client_transfer_dir_t I2C1_TransferDirGet (void)
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
-
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void)
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
-
void I2C1_CallbackRegister (bool(*callback)(i2c_client_transfer_event_t clientEvent))
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
-
void I2C1_Tasks (void)
his function is common Polling function for all I2C1 client. I2C1_Initialize() must have been called for the associated.
Variables
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
-
static volatile uint16_t i2c1Addr
-
static volatile i2c_client_error_ti2c1ErrorState
-
static bool(* I2C1_InterruptHandler )(i2c_client_transfer_event_t clientEvent) = NULL
Detailed Description
This file contains the driver code for I2C1 module.
MSSP1 Generated Driver File
Function Documentation
I2C1_EventHandler()
static void I2C1_EventHandler (void )[static]
Section: Private functions declaration
Section: Private functions
Variable Documentation
i2c1Addr
volatile uint16_t i2c1Addr[static]
Section: Private Variable Definitions
4.15.3.6.6 source/mssp_client_polling.h File Reference
#include <stdbool.h> #include <stdint.h> #include "i2c_client_interface.h"
Functions
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
void I2C1_WriteByte (uint8_t wrByte)
This function writes data to a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint8_t I2C1_ReadByte (void)
This function read data from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
uint16_t I2C1_ReadAddr (void)
This function read requested address from a host on the bus. I2C1_Initialize() must have been called for the associated.
-
i2c_client_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
i2c_client_transfer_dir_t I2C1_TransferDirGet (void)
This function get the I2C Transfer direction. I2C1_Initialize() must have been called for the associated.
-
i2c_client_ack_status_t I2C1_LastByteAckStatusGet (void)
This function get the I2C Host ACK status. I2C1_Initialize() must have been called for the associated.
-
void I2C1_CallbackRegister (bool(*callback)(i2c_client_transfer_event_t clientEvent))
This function sets the pointer to be called "back" when the given I2C transfer events, Bus collision and Write collision occur.
-
void I2C1_Tasks (void)
his function is common Polling function for all I2C1 client. I2C1_Initialize() must have been called for the associated.
Macros
-
#define I2C_Client_InitializeI2C1_Initialize
-
#define I2C_Client_DeinitializeI2C1_Deinitialize
-
#define I2C_Client_WriteByteI2C1_WriteByte
-
#define I2C_Client_ReadByteI2C1_ReadByte
-
#define I2C_Client_ReadAddrI2C1_ReadAddr
-
#define I2C_Client_ErrorGetI2C1_ErrorGet
-
#define I2C_Client_TransferDirGetI2C1_TransferDirGet
-
#define I2C_Client_LastByteAckStatusGetI2C1_LastByteAckStatusGet
-
#define I2C_Client_CallbackRegisterI2C1_CallbackRegister
-
#define I2C_Client_TasksI2C1_Tasks
Variables
-
const struct I2C_CLIENT_INTERFACE I2C_Client
External object for I2C_Client.
Detailed Description
MSSP1 Generated Driver API Header File
Macro Definition Documentation
i2c_client_client_interface
#define i2c_client_client_interface I2C_Client
Section: Data Type Definitions
4.15.3.6.7 source/mssp_host_interrupt.c File Reference
This file contains the driver code for I2C1 module.
#include <xc.h> #include "../mssp1.h"
Functions
-
static void I2C1_ReadStart (void)
-
static void I2C1_WriteStart (void)
-
static void I2C1_Close (void)
-
static void I2C1_EventHandler (void)
-
static void I2C1_ErrorEventHandler (void)
-
static void I2C1_DefaultCallback (void)
-
static uint8_t I2C1_DataReceive (void)
-
static void I2C1_DataTransmit (uint8_t data)
-
static void I2C1_BusReset (void)
-
static void I2C1_ReceiveEnable (void)
-
static void I2C1_RestartEnable (void)
-
static void I2C1_RestartDisable (void)
-
static void I2C1_StartSend (void)
-
static void I2C1_StopSend (void)
-
static void I2C1_AckSend (void)
-
static void I2C1_NackSend (void)
-
static bool I2C1_IsNack (void)
-
static bool I2C1_IsData (void)
-
static bool I2C1_IsAddr (void)
-
static bool I2C1_IsRxBufFull (void)
-
static void I2C1_InterruptsEnable (void)
-
static void I2C1_InterruptsDisable (void)
-
static void I2C1_InterruptClear (void)
-
static void I2C1_ErrorInterruptClear (void)
-
static void I2C1_StatusFlagsClear (void)
-
static i2c_host_event_states_t I2C1_EVENT_IDLE (void)
-
static i2c_host_event_states_t I2C1_EVENT_SEND_RD_ADDR (void)
-
static i2c_host_event_states_t I2C1_EVENT_SEND_WR_ADDR (void)
-
static i2c_host_event_states_t I2C1_EVENT_TX (void)
-
static i2c_host_event_states_t I2C1_EVENT_RX (void)
-
static i2c_host_event_states_t I2C1_EVENT_NACK (void)
-
static i2c_host_event_states_t I2C1_EVENT_ERROR (void)
-
static i2c_host_event_states_t I2C1_EVENT_STOP (void)
-
static i2c_host_event_states_t I2C1_EVENT_RESET (void)
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
bool I2C1_Write (uint16_t address, uint8_t *data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_Read (uint16_t address, uint8_t *data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_WriteRead (uint16_t address, uint8_t *writeData, size_t writeLength, uint8_t *readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
-
i2c_host_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
bool I2C1_IsBusy (void)
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
-
void I2C1_CallbackRegister (void(*callbackHandler)(void))
Setter function for I2C interrupt callback, This will be called when any error is generated.
-
void I2C1_ISR ()
This function is common ISR function for all I2C1 interrupts. I2C1_Initialize() must have been called for the associated.
-
void I2C1_ERROR_ISR ()
This function is common ISR function for all I2C1 Error interrupts. I2C1_Initialize() must have been called for the associated.
Typedefs
-
typedef i2c_host_event_states_t(* i2c1eventHandler) (void)
Variables
-
const i2c_host_interface_t I2C1_Host
External object for I2C1_Host.
-
static void(* I2C1_Callback )(void) = NULL
-
volatile i2c_host_event_status_t i2c1Status = {0}
-
const i2c1eventHandler i2c1_eventTable []
Detailed Description
This file contains the driver code for I2C1 module.
MSSP1 Generated Driver File
Variable Documentation
i2c1_eventTable
const i2c1eventHandler i2c1_eventTable[]
Initial value:
= { I2C1_EVENT_IDLE, I2C1_EVENT_SEND_RD_ADDR, I2C1_EVENT_SEND_WR_ADDR, I2C1_EVENT_TX, I2C1_EVENT_RX, I2C1_EVENT_NACK, I2C1_EVENT_ERROR, I2C1_EVENT_STOP, I2C1_EVENT_RESET }
4.15.3.6.8 source/mssp_host_interrupt.h File Reference
#include <stdio.h> #include <stdint.h> #include <stdbool.h> #include "i2c_host_event_types.h" #include "i2c_host_interface.h"
Functions
-
void I2C1_Initialize (void)
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
-
bool I2C1_Write (uint16_t address, uint8_t *data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_Read (uint16_t address, uint8_t *data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_WriteRead (uint16_t address, uint8_t *writeData, size_t writeLength, uint8_t *readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
-
i2c_host_error_t I2C1_ErrorGet (void)
This function get the error occurred during I2C Transmit and Receive.
-
bool I2C1_IsBusy (void)
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
-
void I2C1_CallbackRegister (void(*callbackHandler)(void))
Setter function for I2C interrupt callback, This will be called when any error is generated.
-
void I2C1_ISR (void)
This function is ISR function for I2C1 Common interrupts.
-
void I2C1_ERROR_ISR (void)
This function is ISR function for I2C1 Error interrupts.
Macros
-
#define i2c1_host_host_interface I2C1_Host
-
#define I2C1_Host_InitializeI2C1_Initialize
-
#define I2C1_Host_DeinitializeI2C1_Deinitialize
-
#define I2C1_Host_WriteI2C1_Write
-
#define I2C1_Host_ReadI2C1_Read
-
#define I2C1_Host_WriteReadI2C1_WriteRead
-
#define I2C1_Host_ErrorGetI2C1_ErrorGet
-
#define I2C1_Host_CallbackRegisterI2C1_CallbackRegister
-
#define I2C1_Host_IsBusyI2C1_IsBusy
Variables
-
const i2c_host_interface_t I2C1_Host
External object for I2C1_Host.
Detailed Description
MSSP1 Generated Driver API Header File
Macro Definition Documentation
i2c1_host_host_interface
#define i2c1_host_host_interface I2C1_Host
Section: Included FilesSection: Data Type Definitions
4.15.3.6.9 source/mssp_host_polling.c File Reference
This file contains the driver code for I2C1 module.
#include <xc.h> #include "../mssp1.h"
Functions
-
static void I2C1_ReadStart (void)
-
static void I2C1_WriteStart (void)
-
static void I2C1_Close (void)
-
static void I2C1_EventHandler (void)
-
static void I2C1_ErrorEventHandler (void)
-
static void I2C1_DefaultCallback (void)
-
static uint8_t I2C1_DataReceive (void)
-
static void I2C1_DataTransmit (uint8_t data)
-
static void I2C1_BusReset (void)
-
static void I2C1_ReceiveEnable (void)
-
static void I2C1_RestartEnable (void)
-
static void I2C1_RestartDisable (void)
-
static void I2C1_StartSend (void)
-
static void I2C1_StopSend (void)
-
static void I2C1_AckSend (void)
-
static void I2C1_NackSend (void)
-
static bool I2C1_IsNack (void)
-
static bool I2C1_IsData (void)
-
static bool I2C1_IsAddr (void)
-
static bool I2C1_IsRxBufFull (void)
-
static void I2C1_InterruptClear (void)
-
static void I2C1_ErrorInterruptClear (void)
-
static void I2C1_StatusFlagsClear (void)
-
static i2c_host_event_states_t I2C1_EVENT_IDLE (void)
-
static i2c_host_event_states_t I2C1_EVENT_SEND_RD_ADDR (void)
-
static i2c_host_event_states_t I2C1_EVENT_SEND_WR_ADDR (void)
-
static i2c_host_event_states_t I2C1_EVENT_TX (void)
-
static i2c_host_event_states_t I2C1_EVENT_RX (void)
-
static i2c_host_event_states_t I2C1_EVENT_NACK (void)
-
static i2c_host_event_states_t I2C1_EVENT_ERROR (void)
-
static i2c_host_event_states_t I2C1_EVENT_STOP (void)
-
static i2c_host_event_states_t I2C1_EVENT_RESET (void)
-
void I2C1_Initialize (void)
This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This routine Deinitializes the I2C1 module. This function disables the module.
-
bool I2C1_Write (uint16_t address, uint8_t *data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_Read (uint16_t address, uint8_t *data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_WriteRead (uint16_t address, uint8_t *writeData, size_t writeLength, uint8_t *readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
-
i2c_host_error_t I2C1_ErrorGet (void)
This function the error occurred during I2C Transmit and Receive. I2C1_Initialize() must have been called for the associated.
-
bool I2C1_IsBusy (void)
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
-
void I2C1_CallbackRegister (void(*callbackHandler)(void))
Setter function for I2C interrupt callback, This will be called when any error is generated.
-
void I2C1_Tasks (void)
his function is common Polling function for all I2C1 client. I2C1_Initialize() must have been called for the associated.
Typedefs
-
typedef i2c_host_event_states_t(* i2c1eventHandler) (void)
Variables
-
const i2c_host_interface_t I2C1_Host
External object for I2C1_Host.
-
static void(* I2C1_Callback )(void) = NULL
-
volatile i2c_host_event_status_t i2c1Status = {0}
-
const i2c1eventHandler i2c1_eventTable []
Detailed Description
This file contains the driver code for I2C1 module.
MSSP1 Generated Driver File
Variable Documentation
i2c1_eventTable
const i2c1eventHandler i2c1_eventTable[]
Initial value:
= { I2C1_EVENT_IDLE, I2C1_EVENT_SEND_RD_ADDR, I2C1_EVENT_SEND_WR_ADDR, I2C1_EVENT_TX, I2C1_EVENT_RX, I2C1_EVENT_NACK, I2C1_EVENT_ERROR, I2C1_EVENT_STOP, I2C1_EVENT_RESET }
4.15.3.6.10 source/mssp_host_polling.h File Reference
#include <stdio.h> #include <stdint.h> #include <stdbool.h> #include "i2c_host_event_types.h" #include "i2c_host_interface.h"
Functions
-
void I2C1_Initialize (void)
This API initializes the I2C1 driver. This routine initializes the I2C1 module. This routine must be called before any other I2C1 routine is called. This routine should only be called once during system initialization.
-
void I2C1_Deinitialize (void)
This API Deinitializes the I2C1 driver. This routine disables the I2C1 module.
-
bool I2C1_Write (uint16_t address, uint8_t *data, size_t dataLength)
This function writes data to a Client on the bus. The function will attempt to write length number of bytes from data buffer to a Client whose address is specified by address. The I2C Host will generate a Start condition,write the data and then generate a Stop Condition. If the Client NACK the request or a bus error was encountered on the bus, the transfer is terminated. The application can call the I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_Read (uint16_t address, uint8_t *data, size_t dataLength)
This function reads the data from a Client on the bus. The function will attempt to read length number of bytes into data buffer from a Client whose address is specified as address. The I2C Host generate a Start condition, read the data and then generate a Stop Condition. If the Client NAKs the request or a bus error is encountered on the bus, the transfer is terminated. The application can call I2C1_ErrorGet() function to know that cause of the error.
-
bool I2C1_WriteRead (uint16_t address, uint8_t *writeData, size_t writeLength, uint8_t *readData, size_t readLength)
This function writes data from the writeData to the bus and then reads data from the Client and stores the received in the readData. The function generates a Start condition on the bus and will then send writeLength number of bytes contained in writeData. The function will then insert a Repeated start condition and proceed to read readLength number of bytes from the client. The received bytes are stored in readData buffer. A Stop condition is generated after the last byte has been received.
-
i2c_host_error_t I2C1_ErrorGet (void)
This function get the error occurred during I2C Transmit and Receive.
-
bool I2C1_IsBusy (void)
This API checks if I2C is busy. I2C must be initialized with I2C1_Initialize() before calling this API.
-
void I2C1_CallbackRegister (void(*callbackHandler)(void))
Setter function for I2C interrupt callback, This will be called when any error is generated.
-
void I2C1_Tasks (void)
This is polling function for non interrupt mode.
Macros
-
#define i2c1_host_host_interface I2C1_Host
-
#define I2C1_Host_InitializeI2C1_Initialize
-
#define I2C1_Host_DeinitializeI2C1_Deinitialize
-
#define I2C1_Host_WriteI2C1_Write
-
#define I2C1_Host_ReadI2C1_Read
-
#define I2C1_Host_WriteReadI2C1_WriteRead
-
#define I2C1_Host_ErrorGetI2C1_ErrorGet
-
#define I2C1_Host_CallbackRegisterI2C1_CallbackRegister
-
#define I2C1_Host_IsBusyI2C1_IsBusy
-
#define I2C1_Host_TasksI2C1_Tasks
Variables
-
const i2c_host_interface_t I2C1_Host
External object for I2C1_Host.
Detailed Description
MSSP1 Generated Driver API Header File
Macro Definition Documentation
i2c1_host_host_interface
#define i2c1_host_host_interface I2C1_Host
Section: Included FilesSection: Data Type Definitions