4.22.2 SPI in MSSP
Serial Peripheral Interface in the Master Synchronous Serial Port
4.22.2.1 Introduction
The Master Synchronous Serial Port (MSSP) peripheral can operate in one of two modes: Serial Peripheral Interface (SPI) and I2C, having the advantage of implementing both communication protocols with the same hardware.
The Serial Peripheral Interface (SPI) module is a synchronous serial data communication bus that operates in Full Duplex mode. In addition, a portable API interface provides a generic SPI interface supporting the MCC Melody Component concept of firmware portability.
4.22.2.2 Supported Device Families
PIC16F152xx | PIC16(L)F153xx | PIC16(L)F188xx | PIC16F171xx |
PIC16F181xx | PIC16F180xx | PIC16(L)F191xx | PIC16(L)F184xx |
PIC16(L)F183xx | PIC16(L)F193x | PIC16(L)F194x | PIC16(L)F178x |
PIC12(L)F182x | PIC16(L)F182x | PIC12(L)F184x | PIC16(L)F184x |
PIC12(L)F161x | PIC16(L)F161x | PIC12(L)F150x | PIC16(L)F150x |
PIC12LF155x | PIC16LF155x | PIC16LF156x | PIC16LF152x |
PIC16(L)F170x | PIC16(L)F171x | PIC16(L)F176x | PIC16(L)F177x |
PIC16(L)F151x | PIC16(L)F145x | ||
PIC18F-K20 | PIC18F-K22 | PIC18F-K40 | PIC18F-K20 |
PIC18F-K50 | PIC18F-K80 | PIC18F-K90 | PIC18F-Q10 |
4.22.2.3 Required header files:
#include "mcc_generated_files/spi/mssp[X].h"
4.22.2.4 Module Documentation
4.22.2.4.1 SPI2
This header file provides API prototypes for the SPI2 driver.
Module description
This header file provides API prototypes for the SPI2 driver.
Data structures
struct SPI_INTERFACE
SPI driver interface object.
Enumerations
enum spi2_configuration_name_t { MSSP2_DEFAULT }
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI2_Open() and is used by the function to set SPI parameters as specified by the configuration.
Functions
void SPI2_Initialize (void)
Initializes the SPI2 module.
void SPI2_Deinitialize (void)
Deinitializes the SPI2 module.
bool SPI2_Open (uint8_t spiConfigIndex)
Enables the SPI2 module with the configurations passed as the parameter. See spi2_config_names_t for the available configurations.
void SPI2_Close (void)
Closes the active configuration of the SPI2 module.
void SPI2_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI2_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI2_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI2_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI2_IsRxReady (void)
Checks if the SPI2 module is ready to read data.
bool SPI2_IsTxReady (void)
Checks if the SPI2 module is ready to write data.
void SPI2_RxCompleteCallbackRegister (void(*CallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer in Interrupt mode.
void SPI2_ISR (void)
Interrupt Service Routine (ISR) for the SPI2 module.
Function Documentation
SPI2_BufferExchange()
void SPI2_BufferExchange (void * bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
in,out | *bufferData |
Buffer address of the data to be exchanged |
in | bufferSize |
Size of the data in bytes |
None. |
SPI2_BufferRead()
void SPI2_BufferRead (void * bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
out | *bufferData |
Buffer address of the data to be read |
in | bufferSize |
Size of the data in bytes |
None. |
SPI2_BufferWrite()
void SPI2_BufferWrite (void * bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
in | *bufferData |
Buffer address of the data to be written |
in | bufferSize |
Size of the data in bytes |
None. |
SPI2_ByteExchange()
uint8_t SPI2_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
byteData |
The byte to be written |
Received data byte |
SPI2_ByteRead()
uint8_t SPI2_ByteRead (void )
Reads one byte of data received in the the SPI buffer.
None. |
Received data byte |
SPI2_ByteWrite()
void SPI2_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
byteData |
The byte to be written |
None. |
To prevent undefined operation of other SPI functions, ensure that the byte received in the SPI buffer is read using SPI2_ByteRead(void).
SPI2_Close()
void SPI2_Close (void )
Closes the active configuration of the SPI2 module.
None. |
None. |
SPI2_Deinitialize()
void SPI2_Deinitialize (void )
Deinitializes the SPI2 module.
None. |
None. |
SPI2_Initialize()
void SPI2_Initialize (void )
Initializes the SPI2 module.
None. |
None. |
SPI2_ISR()
void SPI2_ISR (void )
Interrupt Service Routine (ISR) for the SPI2 module.
None. |
None. |
SPI2_IsRxReady()
bool SPI2_IsRxReady (void )
Checks if the SPI2 module is ready to read data.
None. |
True |
SPI2 module has data ready in buffer |
False |
SPI2 module is not ready to read data |
SPI2_IsTxReady()
bool SPI2_IsTxReady (void )
Checks if the SPI2 module is ready to write data.
None. |
True |
SPI2 module is ready to write data |
False |
SPI2 module is not ready to write data |
SPI2_Open()
bool SPI2_Open (uint8_t spiConfigIndex)
Enables the SPI2 module with the configurations passed as the parameter. See spi2_config_names_t for the available configurations.
spiConfigIndex |
Configuration |
True |
SPI2 module is enabled successfully with the chosen configuration |
False |
SPI2 module is already open with another configuration |
SPI2_RxCompleteCallbackRegister()
void SPI2_RxCompleteCallbackRegister (void(*)(void) CallbackHandler)
Sets the callback function to be executed at the completion of data transfer in Interrupt mode.
Pointer |
to the function to be executed |
None. |
Enumeration Type Documentation
spi2_configuration_name_t
enum enum spi2_configuration_name_t
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI2_Open() and is used by the function to set SPI parameters as specified by the configuration.
MSSP2_DEFAULT |
4.22.2.4.2 SPI1
This header file provides API prototypes for the SPI1 driver.
Module description
This header file provides API prototypes for the SPI1 driver.
Data structures
struct SPI_INTERFACE
SPI driver interface object.
Enumerations
enum spi1_configuration_name_t { MSSP1_DEFAULT }
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI1_Open() and is used by the function to set SPI parameters as specified by the configuration.
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI1_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
bool SPI1_IsTxReady (void)
Checks if the SPI1 module is ready to write data.
Function Documentation
SPI1_BufferExchange()
void SPI1_BufferExchange (void * bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
in,out | *bufferData |
Buffer address of the data to be exchanged |
in | bufferSize |
Size of the data in bytes |
None. |
SPI1_BufferRead()
void SPI1_BufferRead (void * bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
out | *bufferData |
Buffer address of the data to be read |
in | bufferSize |
Size of the data in bytes |
None. |
SPI1_BufferWrite()
void SPI1_BufferWrite (void * bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
in | *bufferData |
Buffer address of the data to be written |
in | bufferSize |
Size of the data in bytes |
None. |
SPI1_ByteExchange()
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
byteData |
The byte to be written |
Received data byte |
SPI1_ByteRead()
uint8_t SPI1_ByteRead (void )
Reads one byte of data received in the the SPI buffer.
None. |
Received data byte |
SPI1_ByteWrite()
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
byteData |
The byte to be written |
None. |
To prevent undefined operation of other SPI functions, ensure that the byte received in the SPI buffer is read using SPI1_ByteRead(void).
SPI1_Close()
void SPI1_Close (void )
Closes the active configuration of the SPI1 module.
None. |
None. |
SPI1_Deinitialize()
void SPI1_Deinitialize (void )
Deinitializes the SPI1 module.
None. |
None. |
SPI1_Initialize()
void SPI1_Initialize (void )
Initializes the SPI1 module.
None. |
None. |
SPI1_IsRxReady()
bool SPI1_IsRxReady (void )
Checks if the SPI1 module is ready to read data.
None. |
True |
SPI1 module has data ready in buffer |
False |
SPI1 module is not ready to read data |
SPI1_IsTxReady()
bool SPI1_IsTxReady (void )
Checks if the SPI1 module is ready to write data.
None. |
True |
SPI1 module is ready to write data |
False |
SPI1 module is not ready to write data |
SPI1_Open()
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
spiConfigIndex |
Configuration |
True |
SPI1 module is enabled successfully with the chosen configuration |
False |
SPI1 module is already open with another configuration |
Enumeration Type Documentation
spi1_configuration_name_t
enum enum spi1_configuration_name_t
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI1_Open() and is used by the function to set SPI parameters as specified by the configuration.
MSSP1_DEFAULT |
4.22.2.4.3 SPI
This header file provides API prototypes for the SPI module in Polling and Interrupt mode.
Module description
This header file provides API prototypes for the SPI module in Polling and Interrupt mode.
This header file provides type definitions for the SPI module operation in Polling mode.
This header file provides type definitions for the SPI module operation in Interrupt mode.
Data structures
struct SPI_INTERFACE
SPI driver interface object.
Enumerations
enum spi_status_t { SPI_RESET = 0x00U, SPI_IDLE = 0x81U, SPI_BUSY = 0x42U }
Enumeration for the different states of the SPI module.
enum spi_transfer_type_t { SPI_READ = 0x00U, SPI_WRITE = 0x81U, SPI_EXCHANGE = 0X42U }
Enumeration for the different transfer types of the SPI module.
Enumeration Type Documentation
spi_status_t
enum enum spi_status_t
Enumeration for the different states of the SPI module.
The enum values are chosen with a specific bit pattern to make sure no error happens in case a single bit changes.
SPI_RESET |
SPI module is in Reset state |
SPI_IDLE |
SPI module is ready to use |
SPI_BUSY |
SPI module is in use |
spi_transfer_type_t
enum enum spi_transfer_type_t
Enumeration for the different transfer types of the SPI module.
The enum values are chosen with a specific bit pattern to make sure no error happens in case a single bit changes.
SPI_READ |
SPI module is performing a read operation |
SPI_WRITE |
SPI module is performing a write operation |
SPI_EXCHANGE |
SPI module is performing an exchange operation |
4.22.2.5 Class Documentation
4.22.2.5.1 spi_configuration_t Struct Reference
#include <spi_interrupt_types.h>
Public Attributes
Member Data Documentation
The documentation for this struct was generated from the following files:
source/
source/
baud
uint8_t baud
clock
uint8_t clock
con1
uint8_t con1
con3
uint8_t con3
stat
uint8_t stat
4.22.2.5.2 spi_descriptor_t Struct Reference
#include <spi_interrupt_types.h>
Public Attributes
uint8_t * buffer
size_t bufferLength
Member Data Documentation
The documentation for this struct was generated from the following file:
source/
buffer
uint8_t* buffer
bufferLength
size_t bufferLength
status
spi_status_t status
transferType
spi_transfer_type_t transferType
4.22.2.5.3 SPI_INTERFACE Struct Reference
SPI driver interface object.
Detailed Description
SPI driver interface object.
SPI Driver prototypes struct.
#include <spi_interface.h>
Public Attributes
void(* Initialize )(void)
void(* Deinitialize )(void)
bool(* Open )(uint8_t spiConfigIndex)
void(* Close )(void)
void(* BufferExchange )(void *bufferData, size_t bufferSize)
void(* BufferRead )(void *bufferData, size_t bufferSize)
void(* BufferWrite )(void *bufferData, size_t bufferSize)
uint8_t(* ByteExchange )(uint8_t byteData)
uint8_t(* ByteRead )(void)
void(* ByteWrite )(uint8_t byteData)
bool(* IsRxReady )(void)
bool(* IsTxReady )(void)
void(* RxCompleteCallbackRegister )(void(*callbackHandler)(void))
void(* TxCompleteCallbackRegister )(void(*callbackHandler)(void))
Member Data Documentation
BufferExchange
void(* BufferExchange) (void *bufferData, size_t bufferSize)
BufferRead
void(* BufferRead) (void *bufferData, size_t bufferSize)
BufferWrite
void(* BufferWrite) (void *bufferData, size_t bufferSize)
ByteExchange
uint8_t(* ByteExchange) (uint8_t byteData)
ByteRead
uint8_t(* ByteRead) (void)
ByteWrite
void(* ByteWrite) (uint8_t byteData)
Close
void(* Close) (void)
Deinitialize
void(* Deinitialize) (void)
Initialize
void(* Initialize) (void)
IsRxReady
bool(* IsRxReady) (void)
IsTxReady
bool(* IsTxReady) (void)
Open
bool(* Open) (uint8_t spiConfigIndex)
RxCompleteCallbackRegister
void(* RxCompleteCallbackRegister) (void(*callbackHandler)(void))
TxCompleteCallbackRegister
void(* TxCompleteCallbackRegister) (void(*callbackHandler)(void))
4.22.2.6 File Documentation
4.22.2.6.1 source/mssp_interrupt.c File Reference
#include <xc.h> #include "../mssp2.h" #include "../spi_interrupt_types.h"
Functions
void SPI2_Initialize (void)
Initializes the SPI2 module.
void SPI2_Deinitialize (void)
Deinitializes the SPI2 module.
bool SPI2_Open (uint8_t spiConfigIndex)
Enables the SPI2 module with the configurations passed as the parameter. See spi2_config_names_t for the available configurations.
void SPI2_Close (void)
Closes the active configuration of the SPI2 module.
void SPI2_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI2_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI2_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI2_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI2_IsRxReady (void)
Checks if the SPI2 module is ready to read data.
bool SPI2_IsTxReady (void)
Checks if the SPI2 module is ready to write data.
void SPI2_ISR (void)
Interrupt Service Routine (ISR) for the SPI2 module.
void SPI2_RxCompleteCallbackRegister (void(*CallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer in Interrupt mode.
Variables
const struct SPI_INTERFACE SPI2
static void(* SPI2_RxCompleteCallback )(void)
static spi_descriptor_t spi2_descriptor
static const spi_configuration_t spi2_configuration []
Variable Documentation
SPI2
const struct SPI_INTERFACE SPI2
Initial value:
= { .Initialize = SPI2_Initialize, .Deinitialize = SPI2_Deinitialize, .Open = SPI2_Open, .Close = SPI2_Close, .BufferExchange = SPI2_BufferExchange, .BufferWrite = SPI2_BufferWrite, .BufferRead = SPI2_BufferRead, .ByteExchange = SPI2_ByteExchange, .ByteWrite = SPI2_ByteWrite, .ByteRead = SPI2_ByteRead, .IsRxReady = SPI2_IsRxReady, .IsTxReady = SPI2_IsTxReady, .RxCompleteCallbackRegister = SPI2_RxCompleteCallbackRegister, .TxCompleteCallbackRegister = NULL }
spi2_configuration
const spi_configuration_t spi2_configuration[][static]
Initial value:
= { { 0x64, 0x4, 0x10, 0x0 } }
spi2_descriptor
spi_descriptor_t spi2_descriptor[static]
Initial value:
= { .buffer = NULL, .bufferLength = 0, .status = SPI_RESET }
SPI2_RxCompleteCallback
void(* SPI2_RxCompleteCallback) (void)[static]
4.22.2.6.2 source/mssp_interrupt.h File Reference
#include "spi_interface.h"
Functions
void SPI2_Initialize (void)
Initializes the SPI2 module.
void SPI2_Deinitialize (void)
Deinitializes the SPI2 module.
bool SPI2_Open (uint8_t spiConfigIndex)
Enables the SPI2 module with the configurations passed as the parameter. See spi2_config_names_t for the available configurations.
void SPI2_Close (void)
Closes the active configuration of the SPI2 module.
void SPI2_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI2_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI2_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI2_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI2_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI2_IsRxReady (void)
Checks if the SPI2 module is ready to read data.
bool SPI2_IsTxReady (void)
Checks if the SPI2 module is ready to write data.
void SPI2_RxCompleteCallbackRegister (void(*CallbackHandler)(void))
Sets the callback function to be executed at the completion of data transfer in Interrupt mode.
void SPI2_ISR (void)
Interrupt Service Routine (ISR) for the SPI2 module.
Enumerations
enum spi2_configuration_name_t { MSSP2_DEFAULT }
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI2_Open() and is used by the function to set SPI parameters as specified by the configuration.
Variables
const struct SPI_INTERFACE SPI2
Variable Documentation
SPI2
const struct SPI_INTERFACE SPI2
4.22.2.6.3 source/mssp_polling.c File Reference
#include <xc.h> #include "../mssp1.h" #include "../spi_polling_types.h"
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI1_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
bool SPI1_IsTxReady (void)
Checks if the SPI1 module is ready to write data.
Variables
const struct SPI_INTERFACE SPI1
static const spi_configuration_t spi1_configuration []
Variable Documentation
SPI1
const struct SPI_INTERFACE SPI1
Initial value:
= { .Initialize = SPI1_Initialize, .Deinitialize = SPI1_Deinitialize, .Open = SPI1_Open, .Close = SPI1_Close, .BufferExchange = SPI1_BufferExchange, .BufferWrite = SPI1_BufferWrite, .BufferRead = SPI1_BufferRead, .ByteExchange = SPI1_ByteExchange, .ByteWrite = SPI1_ByteWrite, .ByteRead = SPI1_ByteRead, .IsRxReady = SPI1_IsRxReady, .IsTxReady = SPI1_IsTxReady, .RxCompleteCallbackRegister = NULL, .TxCompleteCallbackRegister = NULL }
spi1_configuration
const spi_configuration_t spi1_configuration[][static]
Initial value:
= { { 0x64, 0x0, 0x10, 0x1 } }
4.22.2.6.4 source/mssp_polling.h File Reference
#include "spi_interface.h"
Functions
void SPI1_Initialize (void)
Initializes the SPI1 module.
void SPI1_Deinitialize (void)
Deinitializes the SPI1 module.
bool SPI1_Open (uint8_t spiConfigIndex)
Enables the SPI1 module with the configurations passed as the parameter. See spi1_config_names_t for the available configurations.
void SPI1_Close (void)
Closes the active configuration of the SPI1 module.
void SPI1_BufferExchange (void *bufferData, size_t bufferSize)
Exchanges the buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferWrite (void *bufferData, size_t bufferSize)
Writes a buffer using the SPI protocol. This function is blocking in Polling mode.
void SPI1_BufferRead (void *bufferData, size_t bufferSize)
Reads a buffer using the SPI protocol. This function is blocking in Polling mode.
uint8_t SPI1_ByteExchange (uint8_t byteData)
Exchanges one byte using the SPI protocol. This function is blocking.
void SPI1_ByteWrite (uint8_t byteData)
Writes one byte to the SPI buffer.
uint8_t SPI1_ByteRead (void)
Reads one byte of data received in the the SPI buffer.
bool SPI1_IsRxReady (void)
Checks if the SPI1 module is ready to read data.
bool SPI1_IsTxReady (void)
Checks if the SPI1 module is ready to write data.
Enumerations
enum spi1_configuration_name_t { MSSP1_DEFAULT }
Enumeration for the different configurations supported by the driver. A configuration is specified as parameter to SPI1_Open() and is used by the function to set SPI parameters as specified by the configuration.
Variables
const struct SPI_INTERFACE SPI1
Variable Documentation
SPI1
const struct SPI_INTERFACE SPI1
4.22.2.6.5 source/spi_interface.h File Reference
#include <stdint.h> #include <stdbool.h> #include <stddef.h>
Data structures
struct SPI_INTERFACE
SPI driver interface object.
Detailed Description
SPI Driver API Interface File
4.22.2.6.6 source/spi_interrupt_types.h File Reference
Data structures
struct spi_descriptor_t
struct spi_configuration_t
Enumerations
enum spi_status_t { SPI_RESET = 0x00U, SPI_IDLE = 0x81U, SPI_BUSY = 0x42U }
Enumeration for the different states of the SPI module.
enum spi_transfer_type_t { SPI_READ = 0x00U, SPI_WRITE = 0x81U, SPI_EXCHANGE = 0X42U }
Enumeration for the different transfer types of the SPI module.
Detailed Description
SPI Type Definitions Header File
4.22.2.6.7 source/spi_polling_types.h File Reference
Data structures
struct spi_configuration_t
Detailed Description
SPI Type Definitions Header File