1 Feature Overview
1.1 BLE Config App Service Component
When regenerating an existing Bluetooth Low Energy (BLE) sample application from scratch, numerous code snippets must be manually inserted into various files before testing the application's functionality. The following steps are followed:
- Configure various components using MCC.
- Generate code by clicking the "Generate" button.
- Manually add code snippets to various files.
- Build the application.
The step of manually adding code snippets to various files is both cumbersome and time-consuming. Additionally, it increases the risk of errors if the code is not copied correctly.
By leveraging the “BLE Config App Service” component, all required code is
automatically generated into app_ble_callbacks.c,
app_ble_callbacks.h, app.c,
app.h, app_utility.c, and
app_utility.h files based on the Bluetooth Low Energy Stack
settings. This enables seamless integration of the code.
Features
- Auto Generation of Code Based on BLE_STACK Settings.
- Selection of MCHP or Custom Board.
- Automatic Generation of Bluetooth Low Energy callback and utility files which enables users to utilize, add, or modify application code without needing to delve into the source files.
For more details on activating and using the “BLE Config App Service” component refer to the Getting Started with WME Bluetooth Low Energy Applications from Related Links.
1.2 WME Application Service Component
WME Application Service components are designed to improve existing profile components by replicating their GUI and incorporating several advanced features. For more details, see WME Application Service Components from Related Links.
1.3 Custom Protocol Service Component with GUI
Custom Protocol Application Service component help users to quickly design custom protocols over Bluetooth Low Energy custom service to their specific requirements. The ability to set custom protocols for characteristics over customized service would significantly enhance user flexibility and comfort. For more details, See Bluetooth Low Energy Custom Protocol Application Service from Related Links.
1.4 Enable App Code Generation
This feature includes an Enable/Disable switch that permits users to manage the generation of application code for a specific profile, as well as based on the configuration of the BLE stack component. When users enable application code generation, the necessary application code functions for the corresponding BLE stack settings and any existing profiles in the project will be generated. These generated application-specific functions will be included in both the generic callback file and the profile-specific callback file.
To illustrate the usage of the Enable App Code, we will use the “ble_ancs_application” as an example.
Files generated by Enable App Code Generation in Enabled state.
1.5 Functions to Handle Event Handlers
During project development, users may need to incorporate business logic into applications for specific Bluetooth Low Energy or Bluetooth Low Energy profile/service events. This requires them to access handler files and add their logic to the relevant events, necessitating knowledge of both handler files and event triggering locations. By offering functions/APIs that follow a callback approach for these events, users can implement their logic directly within the callback functions, eliminating the need to manage handler files.
To illustrate, ‘ble_ancs_application’ is used as an example
app_ble_handler.capp_ble_callbacks.capp_ancs_handler.capp_ancs_callbacks.c1.6 Reduced Dependencies and Satisfiers Pop-up Messages
In the current project interface, when users drag and drop components such as the Bluetooth Low Energy Stack or any Profile components, dialogue boxes appear prompting them to confirm the addition or removal of dependent components. Users must add these dependent components, but the dialogue boxes may inadvertently allow them to skip this step. Furthermore, these mandatory dialogue pop-ups could negatively impact the user experience. Implementing WME and utilizing its components will result in fewer pop-up messages, thereby reducing the likelihood of users accidentally disabling or skipping components.
1.7 Auto Detect Existing BLE MCC Components and Generation of Application Code
Using the WME framework, the BLE App Config component and profile can detect existing Bluetooth Low Energy components and their settings, and subsequently generating application code based on those settings. For more information, refer to the following chapters from Related Links.
- BLE Config App Service Component
- WME Application Service Component
- Auto Configuration of BLE Stack
- Enable App Code Generation
1.8 Auto Configuration of BLE Stack
Upon activating the Profile App Service, the component stack will be automatically configured to meet the application's specific requirements based on the selected service configuration. To illustrate this feature, consider the Apple Notification App Service component. The image below shows the automatic configuration performed by the Apple Notification App Service. Users can view the auto-configured items highlighted in blue within the GUI.
1.9 Segregation of all MCC Configuration Items
into configuration.h File
In the current implementation of all the Bluetooth® Low Energy MCC
components, the values set by the user in the configuration option are directly used
within the functions as hard-coded values. Similarly, Bluetooth Low Energy stack macros
are defined in their respective header files such as ble_gap.h,
ble_l2cap.h, ble_smp.h, gatt.h,
and so on., and are assigned directly to the variable in application files. Implementing
the WME framework and utilizing its components will result in the segregation of MCC
configuration items into a single file (configuration.h), thereby
eliminating all hard-coded numbers. The images below illustrate the file changes before
and after the implementation of the WME framework for Bluetooth Low Energy stack
configuration.
app_ble.c File)app_ble.c File)configuration.h File1.10 Reduced Number of Application Files
In the current implementation of the applications, several additional files related to
Bluetooth Low Energy functionality, Bluetooth Low Energy profile-specific functionality,
and non-Bluetooth Low Energy functionality are distributed throughout the
src folder. The WME framework consolidates all code in these files
into app_ble_callbacks.c,
app_<profile>_callbacks.c, where <profile> may
refer to ANCS, ANPS, so on., and app_utility.c. This reorganization
simplifies the process for users, as they no longer need to search through multiple
files to determine where to add or modify their code.
For example, in the ble_throughput_app, the highlighted files have been
removed, and their code has been transferred to the corresponding callbacks file.
1.11 No User Code Inside app_ble.c
and Reduced Merge Conflicts
In the existing implementation, the values set by the user in the Bluetooth Low Energy
Stack component configuration options are directly used within the functions as
hard-coded values. Similarly, Bluetooth Low Energy Stack macros are defined in their
respective header files, such as ble_gap.h,
ble_l2cap.h, ble_smp.h, gatt.h
and so on., and are directly assigned to variables in the application files. All these
actions occur in app_ble.c. When the user modifies the
app_ble.c file and changes the Bluetooth Low Energy Stack
configurations, there is a high likelihood of merge conflicts, which can lead to user
confusion and the potential omission of code pieces while resolving these conflicts.
With the WME framework, users are not permitted to make any changes to
app_ble.c, and all Bluetooth Low Energy-related macros are
generated in configuration.h. This approach significantly reduces the
risk of merge conflicts.
- Without WME
-
In the current implementation, the user edits the
app_ble.cfile.Figure 1-24. User Code in app_ble.c - The user changes BLE Stack settings.
Figure 1-25. BLE Stack Settings - After generation, merge
conflicts appear.
Figure 1-26. Merge Conflict
-
- With WME
- In WME framework, instead of
modifying
app_ble.c, user modifiesconfiguration.h. - After modifying the BLE Stack
settings and generating the necessary files, a merge suggestion appears for
configuration.h, making it easy for the user to proceed with the merges.Figure 1-27. Merge Suggestions
- In WME framework, instead of
modifying
1.12 System Hardware Definitions support
System Hardware Definitions (SHD) offers a user-friendly interface through MCC, allowing users to automatically configure hardware settings and dependencies with a simple click in the board settings. Utilizing the WME framework, users can select the SHD component based on the device from the BLE Config App Service component and configure pins or enable peripherals according to the Development/Evaluation Boards in Microchip. For more information on how to activate SHD from the BLE Config App Service component, see Getting Started with WME Bluetooth Low Energy Applications from Related Links.
1.13 Debug Prints Instead of Console Prints
While the Console service component is useful for basic input/output
operations and simple debugging tasks, the Debug service
component offers a more comprehensive and powerful set of tools
for in-depth debugging and diagnostics. Developers working on
complex or performance-critical applications will likely benefit
more from the advanced features provided by the Debug service
component. The Debug service supports different system-defined
Debug Levels (SYS_ERROR_FATAL,
SYS_ERROR_ERROR,
SYS_ERROR_WARNING,
SYS_ERROR_INFO,
SYS_ERROR_DEBUG), allowing messages
to be filtered based on their severity. This feature helps in
controlling the verbosity of the debug output.
1.14 Utility Functions for Advertising/Scan Response Data
Utility functions for Advertising and Scan Response data dynamically update the service data and user data of those packets through the application code, rather than through the stack configuration GUI, which employs macro configuration on the generated code. The system will generate these utility functions in all cases; however, users need to employ these functions when Legacy Advertisement is used.
Utility APIs
The APIs are detailed
in the section below and can be found in the app_utility file. These APIs
append or insert user input data into the appropriate locations within the advertisement or
scan response packets, which are generated from the GUI.
APP_UTILITY_UpdateBleAdvServiceData()- Description: Append data on
Bluetooth Low Energy service data of the advertising packet, which comes from the GUI
configuration.
Table 1-1. Parameters Param Description p_svcDataPointer to the uint8_tbuffer, this buffer data will be appended on Bluetooth Low Energy service data of advertising packetsvcDataLenLength of the buffer Table 1-2. Return Value Return Val Description APP_UTILITY_SUCCESSSuccessfully appended to service data. APP_UTILITY_INVALID_LENAppend operation not allowed due to invalid length. APP_UTILITY_FAILAppend failure due to stack API call returned a failure.
- Description: Append data on
Bluetooth Low Energy service data of the advertising packet, which comes from the GUI
configuration.
APP_UTILITY_UpdateBleAdvUserData()- Description: Append data on
Bluetooth Low Energy user data of the advertising packet, which comes from the GUI
configuration.
Table 1-3. Parameters Param Description p_userDataPointer to the uint8_tbuffer, this buffer data will be appended on Bluetooth Low Energy user data of advertising packet.userDataLenLength of the buffer Table 1-4. Return Value Return Val Description APP_UTILITY_SUCCESSSuccessfully appended to service data. APP_UTILITY_INVALID_LENAppend operation not allowed due to invalid length. APP_UTILITY_FAILAppend failure due to stack API call returned a failure.
- Description: Append data on
Bluetooth Low Energy user data of the advertising packet, which comes from the GUI
configuration.
APP_UTILITY_UpdateBleScanRspServiceData()- Description: Append data on
Bluetooth Low Energy user data of the scan response packet, which comes from the GUI
configuration.
Table 1-5. Parameters Param Description p_svcDataPointer to the uint8_tbuffer, this buffer data will be appended on Bluetooth Low Energy service data of the scan response packet.svcDataLenLength of the buffer Table 1-6. Return Value Return Val Description APP_UTILITY_SUCCESSSuccessfully appended to service data. APP_UTILITY_INVALID_LENAppend operation not allowed due to invalid length. APP_UTILITY_FAILAppend failure due to stack API call returned a failure.
- Description: Append data on
Bluetooth Low Energy user data of the scan response packet, which comes from the GUI
configuration.
APP_UTILITY_UpdateBleScanRspUserData- Description: Append data on
Bluetooth Low Energy user data of the scan response packet,which comes from the GUI
configuration.
Table 1-7. Parameters Param Description p_userDataPointer to the uint8_tbuffer, this buffer data will be appended on Bluetooth Low Energy user data of the scan response packet.userDataLenLength of the buffer Table 1-8. Return Value Return Val Description APP_UTILITY_SUCCESSSuccessfully appended to service data. APP_UTILITY_INVALID_LENAppend operation not allowed due to invalid length. APP_UTILITY_FAILAppend failure due to stack API call returned a failure.
- Description: Append data on
Bluetooth Low Energy user data of the scan response packet,which comes from the GUI
configuration.
Example Usage for Appending Service Data
All static data for advertising and scan response must be provided through the GUI by enabling the respective fields if they are being used. For instance, the user is configuring service data in the advertising data as illustrated in the following figure.
In the above image, the service UUID is DAFE and the service data is FF01, which are static values. If the user wishes to append dynamic values to the service data at the end of FF01, they can use the update service data API after the Bluetooth Low Energy stack initialization. After calling the API, the user needs to re-enable the advertisement to restart it with the updated packet. For example, if the user wants to append "020304" to the service data along with FF01, they can use the following code:
uint8_t appendServiceData[]={0x02,0x03,0x04};
APP_UTILITY_UpdateBleAdvServiceData(appendServiceData,3);
BLE_GAP_SetAdvEnable(0x01, 0x00);This code will append 020304 to the FF01 service
data, updating it to FF01020304. If the user wants to dynamically update the entire service
data, they must leave the service data field blank instead of using FF01 or any default
value (the default value is 00, which must be removed to leave the field blank). Similarly,
users can append service data in the scan response by using the respective API.Example Usage for Appending User Data
As mentioned in the above section, first user need to configure all static data. For instance, the user wants to configure entire user defined data dynamically. For this user defined data must not be enabled or user defined data field must be blank as in the below image.
To add user-defined hex data "03031118," the user can utilize the following code:
uint8_t appendUserData[]={0x03,0x03,0x11,0x18};
APP_UTILITY_UpdateBleAdvUserData(appendServiceData,4);
BLE_GAP_SetAdvEnable(0x01, 0x00);
Similarly, users can append user data in the scan response by using the respective API.