1 Flash Memory
The Flash memory on dsPIC33AK256MPS306 family devices is divided into quadwords (16 bytes each), write rows (512 bytes each) and erase pages (4096 bytes each). The quadword (four 32-bit long words) is the minimum data size that can be written into the Flash. The address of each quadword is aligned by 16 bytes. The Flash memory can be written by rows, and each row consists of 32 quadwords or 512 bytes. The address of each row is aligned by 512-byte boundaries.
The Flash memory must be erased before a write operation can be initiated, and it can be erased by pages. Each erase page consists of eight rows or 4096 bytes. The address of each erase page is aligned by 4096-byte boundaries.
The dsPIC33AK256MPS306 family devices’ Flash memory regions are shown in Table 1-1.
| Memory Region | Address | Number of Quadwords | Number of Write Rows | Number of Erase Pages | Description | ||
|---|---|---|---|---|---|---|---|
| User OTP | 0x7F2C00-0x7F3000 | 64 | 2 | Not applicable | Quadword or row programmed, never erasable | ||
| User Configuration A (UCA1) | 0x7F3000-0x7F3FFC | 256 | 8 | 1 | Bulk or page erased, quadword programmed | ||
| User Configuration B (UCB) | 0x7F4000-0x7F4FFC | 256 | 8 | 1 | |||
| User Configuration A2 (UCA2) | 0x7FB000-0x7FBFFC | 256 | 8 | 1(1) | |||
| Code Memory | 128-Kbyte Flash Memory Devices | Single Boot | 800000-81FFFC | 8182 | 256 | 32 | Bulk or page erased, quadword or row programmed |
| Dual Boot | 800000-80FFFC | 4091 | 128 | 16 | |||
| C00000-C0FFFC | 4091 | 128 | 16 | ||||
| 256-Kbyte Flash Memory Devices | Single Boot | 800000-83FFFC | 16384 | 512 | 64 | ||
| Dual Boot | 800000-81FFFC | 8182 | 256 | 32 | |||
| C00000-C1FFFC | 8182 | 256 | 32 | ||||
|
Note:
| |||||||
Some dsPIC33AK256MPS306 family device registers are used in the programming procedures. The descriptions and addresses of these registers are listed in Table 1-2.
| Register Name | Address | Description |
|---|---|---|
| VISI | 0x0007C0 | This is a register to move (shift) data out of the device through the ICSP interface. |
| NVMCON | 0x003000 | This is a register to select type and initiate erase or write Flash operations. |
| NVMADR | 0x003004 | This register is the destination Flash address for erase or write operations. |
| NVMDATA0 | 0x003008 | This is a register with data to be programmed to Flash when quadword write is used. |
| NVMDATA1 | 0x00300C | This is a register with data to be programmed to Flash when quadword write is used. |
| NVMDATA2 | 0x003010 | This is a register with data to be programmed to Flash when quadword write is used. |
| NVMDATA3 | 0x003014 | This is a register with data to be programmed to Flash when quadword write is used. |
| NVMSRCADR | 0x003018 | This register should be set to the address of the RAM buffer loaded with the Flash row data to be programmed. |
| NVMCRCCON | 0x003048 | This register controls the Cyclic Redundancy Check (CRC) calculation of the Flash region. |
| NVMCRCST | 0x00304C | This register contains the start address of the 4-Kbyte Flash memory block for the CRC calculation. |
| NVMCRCEND | 0x003050 | This register contains the end address of the 4-Kbyte Flash memory block minus one byte for the CRC calculation. |
| NVMCRCSEED | 0x003054 | The initial CRC value (seed) should be loaded into this register. If the CRC-32 is calculated for the multiple memory blocks, then the previous CRC result must be written directly to NVMCRCSEED before the next block of CRC calculations. |
| NVMCRCDATA | 0x003058 | This register contains the CRC calculation result. |