1.23.1.26 ADCHS_ComparatorxCallbackRegister Function
C
void ADCHS_ComparatorxCallbackRegister(ADCHS_DC_CALLBACK callback, uintptr_t context) // x - Comparator number
Summary
Registers the function to be called from the ADC comparator interrupt
Description
This function registers the callback function to be called from the ADC comparator interrupt
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointer to the callers context for multi-instance clients) |
Returns
None.
Example
void ADCHS_Comparator1_Callback_Fn(ADCHS_CHANNEL_NUM channel, uintptr_t context)
{
}
ADCHS_Comparator1CallbackRegister(ADCHS_Comparator1_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.