1.23.1.24 ADCHS_ComparatorxEventModeSet Function
C
void ADCHS_ComparatorxEventModeSet(ADCHS_CMP_EVENT_MODE eventMode) // x - Comparator number
Summary
Sets the condition under which the comparator output becomes true
Description
Sets the condition under which the comparator output becomes true
Precondition
ADCHS_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
eventMode | A logical OR of the following events: ADCHS_CMP_EVENT_MODE_IELOLO ADCHS_CMP_EVENT_MODE_IELOHI ADCHS_CMP_EVENT_MODE_IEHILO ADCHS_CMP_EVENT_MODE_IEHIHI ADCHS_CMP_EVENT_MODE_IEBTWN |
Returns
None
Example
ADCHS_Comparator1EventModeSet(ADCHS_CMP_EVENT_MODE_IELOHI | ADCHS_CMP_EVENT_MODE_IEHIHI);
Remarks
None