1.27.2.8 ADC_ChannelResultGet Function
C
uint16_t ADC_ChannelResultGet (ADC_CHANNEL channel) uint16_t ADC_ChannelResultGet (ADC_CHANNEL_NUM channel)
Summary
Reads the conversion result of the channel
Description
This function reads the conversion result of the channel
Precondition
ADC_Initialize() must have been called first for the associated instance. And conversion must have been started.
Parameters
Param | Description |
---|---|
channel | channel number |
Returns
uint16_t - conversion result
Example
uint16_t result; bool status; ADC_Initialize(); ADC_ChannelsEnable(ADC_CH0); ADC_ConversionStart(); status = ADC_ChannelResultIsReady(ADC_CH0); if (status) { result = ADC_ChannelResultGet(ADC_CH0); }
Remarks
This function can be called from interrupt or by polling the status when result is available. User should decode the result based on result sign mode (signed or unsigned result) and result resolution (12, 13 or 14 bit result) configuration.