1.32.20.18 PORT_PinPeripheralFunctionConfig Function

C

void PORT_PinPeripheralFunctionConfig(PORT_PIN pin, PERIPHERAL_FUNCTION function)

Summary

Configures the peripheral function on the selected port pin

Description

This function configures the given peripheral function on the selected port pin.

Precondition

The PORT_Initialize() function should have been called.

Parameters

Param Description
pin One of the IO port pin from the enum PORT_PIN
function One of the peripheral functions from the enum PERIPHERAL_FUNCTION

Returns

None.

Example

// Enable Peripheral function B on port pin PB01
PORT_PinPeripheralFunctionConfig(PORT_PIN_PB01, PERIPHERAL_FUNCTION_B);

Remarks

None.