1.3.22.30 RTC_Timer16CounterHasOverflowed Function
C
bool RTC_Timer16CounterHasOverflowed ( void )
Summary
Checks if the 16-bit counter has overflowed
Description
This function returns true if the counter value has matched the configured 16-bit timer period. The counter will be reset and start counting again.
The API can be used to poll period completion when using the timer counter as a timer. Calling the function will clear the internal period match flags if these flags were set at the time of calling the function.
Precondition
RTC_Initialize, RTC_Timer16Start and RTC_Timer16PeriodSet must have been called for the associated RTC instance. The RTC peripheral should have been configured in 16-bit Timer Counter mode.
Parameters
None.
Returns
True, if counter has overflowed, False otherwise.
Example
bool counterOverflowed = false; RTC_Initialize(); RTC_Timer16PeriodSet(0x3000); RTC_Timer16CounterSet(0); RTC_Timer16Start(); do { counterOverflowed = RTC_Timer16CounterHasOverflowed(); }
Remarks
None.