1.30.8.1 EVSYS_UserEnable Function

C

void EVSYS_UserEnable(EVSYS_CHANNEL channel, uint8_t user)

Summary

Enables EVSYS user

Description

This function enables the specified EVSYS user.

Precondition

EVSYS module should be initialized with the required configuration parameters from the MHC GUI in the EVSYS_Initialize() function

Parameters

Param Description
channel Channel for which the user needs to be enabled
user User to be enabled

Returns

None

Example

// Enable Event System user 1 for Event Channel 0
EVSYS_UserEnable(EVSYS_CHANNEL_0, 1);

Remarks

The EVSYS_UserEnable API should be used to enable user at run time.