1.37.17.3 TCCx_Timer16bitCounterGet Function

C

/* x = TCC instance number */
uint16_t TCCx_Timer16bitCounterGet( void );

Summary

Reads the timer current count value.

Description

This function reads the timer count value.

Precondition

TCCx_TimerInitialize() function must have been called first.

Parameters

None.

Returns

Timer's current count value.

Example

uint16_t counter = 0;
TCC0_TimerInitialize();
TCC0_TimerStart();
counter = TCC0_Timer16bitCounterGet();

Remarks

The caller must know the number of significant bytes of timer. Period value is right-aligned.