1.27.3.3 AIC_INT_IrqDisable Function

C

bool AIC_INT_IrqDisable ( void )

Summary

Disable interrupt to the processor.

Description

AIC will not generate interrupts to the processor when an interrupt condition is met.

Precondition

AIC should be initialized with a call to AIC_Initialize() function.

Parameters

None.

Returns

Current interrupt state.

Example

bool state = AIC_INT_IrqDisable ( );

Remarks

None.