1.41.21.1 TCx_CHy_TimerInitialize Function
C
/* x = TC instance number, y= channel number */ void TCx_CHy_TimerInitialize ( void );
Summary
Initializes given instance of TC channel
Description
This function initializes given instance of TC channel in timer mode with the options configured in MCC GUI.
Precondition
MCC GUI should be configured with the desired values.
Parameters
None.
Returns
None.
Example
TC1_CH0_TimerInitialize();
Remarks
This function must be called before any other TC function is called. This function is normally only be called once during system initialization.