1.34.29.7 XDMACn_ChannelDisable Function
C
// n is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral. void XDMACn_ChannelDisable (XDMAC_CHANNEL channel)
Summary
Disables the specified channel.
Description
This function disables the specified channel and resets it. Ongoing transfer will be aborted.
Precondition
XDMAC should have been initialized by calling XDMACn_Initialize. And transfer should have been initiated.
Parameters
Param | Description |
---|---|
channel | A specific XDMAC channel |
Returns
None.
Example
XDMAC_ChannelDisable(XDMAC_CHANNEL_1);
Remarks
None.