1.34.29.2 XDMACn_ChannelCallbackRegister Function
C
// n is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral. void XDMACn_ChannelCallbackRegister ( XDMAC_CHANNEL channel, const XDMAC_CHANNEL_CALLBACK eventHandler, const uintptr_t contextHandle )
Summary
This function allows a XDMAC PLIB client to set an event handler.
Description
This function allows a client to set an event handler. The client may want to receive transfer related events in cases when it submits a XDMAC PLIB transfer request. The event handler should be set before the client intends to perform operations that could generate events.
This function accepts a contextHandle parameter. This parameter could be set by the client to contain (or point to) any client specific data object that should be associated with this XDMAC channel.
Precondition
XDMAC should have been initialized by calling XDMACn_Initialize.
Parameters
Param | Description |
---|---|
channel | A specific XDMAC channel from which the events are expected. |
eventHandler | Pointer to the event handler function. |
contextHandle | Value identifying the context of the application/driver/middleware that registered the event handling function. |
Returns
None.
Example
MY_APP_OBJ myAppObj;
void APP_XDMACTransferEventHandler(XDMAC_TRANSFER_EVENT event,
uintptr_t contextHandle)
{
switch(event)
{
case XDMAC_TRANSFER_COMPLETE:
// This means the data was transferred.
break;
case XDMAC_TRANSFER_ERROR:
// Error handling here.
break;
default:
break;
}
}
// User registers an event handler with XDMAC channel. This is done once.
XDMAC_ChannelCallbackRegister(channel, APP_XDMACTransferEventHandler,
(uintptr_t)&myAppObj);
Remarks
None.