1.29.2.6 ADCx_ConversionStatusGet Function
C
bool ADCx_ConversionStatusGet( void ); // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Returns the status of the conversion of the channel.
Description
This function returns the status of whether channel conversion is complete
Precondition
ADCx_Initialize() function must have been called first for the associated instance. Also conversion must have been started.
Parameters
None.
Returns
false - Conversion is not finished or not started yet true - Conversion is complete
Example
bool adcConversionStatus = false; ADC0_Initialize(); ADC0_ConversionStart(); adcConversionStatus = ADC0_ConversionStatusGet();
Remarks
This function should be called only after conversion is started.