1.41.4.4 DACC_ChannelSelect Function

C

void DACC_ChannelSelect(DACC_CHANNEL_NUM channel)

Summary

Select the channel of DACC module for new conversion request

Description

This function selects the channel of DACC module for new conversion request.

Precondition

DACC_Initialize must have been called for the associated DACC instance.

Parameters

Param Description
channel Points to DACC Channel

Returns

None.

Example

bool status = false;
DACC_ChannelSelect(DACC_CHANNEL_0);
if (true == DACC_IsReady())
{
    DACC_DataWrite (0xff);
}
else
{
    //DACC is not ready to accept new conversion request
    //User Application code
}

Remarks

None.