1.5.26.1 SUPC_Initialize Function

C

void SUPC_Initialize( void );

Summary

Initializes the SUPC peripheral.

Description

This function initializes the SUPC peripheral of the device with the values configured in MHC GUI.

Precondition

MHC GUI should be configured with the right values.

Parameters

None.

Returns

None.

Example

SUPC_Initialize();

Remarks

This function should only be called once during system initialization before any other SUPC function is called.