1.34.5.1 EFC_Initialize Function

C

void EFC_Initialize( void )

Summary

Initializes given instance of the EFC peripheral.

Description

This function initializes the given instance of the EFC peripheral as configured by the user from within the MHC.

Precondition

None.

Parameters

None.

Returns

None.

Example

EFC_Initialize();

Remarks

This function should be called before calling any other EFC library function.