1.29.22.10 SDADC_CallbackRegister Function
C
void SDADC_CallbackRegister(SDADC_CALLBACK callback, uintptr_t context)
Summary
Registers the function to be called from interrupt.
Description
This function registers the callback function to be called from interrupt.
Precondition
SDADC_Initialize() must have been called first.
Parameters
Param | Description |
---|---|
callback | callback function pointer |
context | Allows the caller to provide a context value (usually a pointerto the callers context for multi-instance clients) |
Returns
None.
Example
void SDADC_Callback_Fn( uintptr_t context );
SDADC_Initialize();
SDADC_CallbackRegister(SDADC_Callback_Fn, NULL);
Remarks
Context value can be set to NULL if not required. To disable callback function, pass NULL for the callback parameter.