1.29.22.8 SDADC_WindowMonitorIsSet Function

C

bool SDADC_WindowMonitorIsSet( void )

Summary

Returns the status of the window monitor.

Description

This function returns the status of whether window monitor condition is met.

Precondition

SDADC_Initialize() function must have been called first for the associated instance. Also conversion must have been started.

Parameters

None.

Returns

true - Window monitor condition is met false - Window monitor condition is not met

Example

bool sdadcWinMonStatus;
SDADC_Initialize();
SDADC_ConversionStart();
sdadcWinMonStatus = SDADC_WindowMonitorIsSet();

Remarks

This function should be called only after conversion is started and window monitor mode is enabled.